This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TIer
Customer needs a power MOS, 30V VDS, hope its CISS can be less than 1500pF, since TI.com does not have a direct filter to use,
Could you recommend an NMOS and PMOS to me? Thanks.
Hello Tony,
Thanks for promoting TI FETs at your customer. TI P-channel FETs only go to -20V max and we do not have any -30V PFETs. The MOSFET product table does not include a filter for CISS. However, you can sort on QG since it is proportional to CISS. You do not mention any current or on resistance requirements - only CISS < 1500pF and BVDSS >= 30V. We have many devices that meet those basic requirements. Please take a look at CSD17571Q2 30V NFET in 2x2mm SON package with CISS = 360pF typical, 468pF max. If you can share more application requirements, it might be easier to narrow down the FET selection.
Best Regards,
John Wallace
TI FET Applications
Hi Tony,
Following up to see if your issue has been resolved. Please let me know.
Thanks,
John
Hi Tony,
Since I have not heard back from, I assume your issue is resolved and will close this thread.
Thanks,
John