Other Parts Discussed in Thread: LM5185, LM5185-Q1
Hi Youhao Xi,
I hope you are doing well,
This is regarding my PSR flyback converter design using LM5185Q1. We are facing constraints at transformer design and costing for the design which I shared you (Please find the attachment). In this case I want to use an off- the shelf transformer part which supports for below output range.
Secondary Output1: 30V 4A
Secondary Output2: Between 7V to 3.6V @ 6W (This voltage will be set based on standard transformer part support)
Please let me know your cost-effective solution and transformer part to ready to use on our application.
Regards,
Ravi