This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: DCHG/DDSG pin status and CHG/DSG FET status

Part Number: BQ76952

Hi,

I wanted to double-check if my understanding about the DCHG and DDSG pins of BQ76952 is correct.

Assumption:

The DCHG/DDSG pins are configured for DCHG/DDSG functionality.

Statement:

Asserted DCHG/DDSG pins confirms that the CHG/DSG FETs are open. However, the CHG/DSG FETs could be either open or closed when the DCHG/DDSG pins are de-asserted.

Is the above statement true? Or do the de-asserted DCHG/DDSG pins always guarantee that the CHG/DSG FETs are closed?

Thank you,

Kyungjae Lee