This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM843620: Need Help to get the reference design

Part Number: TPSM843620


Hi,
We are using TPSM843620 in our design. when we try to make the circuit with the help of webench  we are getting the following error

 I am not able to Simulate the design to get the required output capacitance to make the circuit in in acceptable ripple range.

Our Design parameters are as follows


Vin 12V((10.8V(min) and 13.2V(max))

Output current 3.1A

Output  voltage  1.2V

Ambient temperature 55C

Kindly Help us here to make the Proper Design

Regards 
Pavan