This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS923654: Is it no problem to use TPS922054/5 to drive under 48Vin and 25Vo/3AIo conditions?

Part Number: TPS923654
Other Parts Discussed in Thread: TPS922052, TPS922054

Hello Steven,

Could I ask you about your reply to the following my question.

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1351434/tps923654-can-tps923654-be-used-for-led-lighting-with-vin-24v-vout-vf-50v-and-io-3-5a-conditions/5166721?tisearch=e2e-sitesearch&keymatch=kazuya#5166721

You said in the thread that You may need to parallel two TPS922052/3 to achieve an output power of Vout(Vf)=50V and Io=3.5A due to thermal limit.

If TJ can be kept less than 125C using air or water cooling system, is it no problem to use TPS922054/5 to drive under new condition, 48Vin and  25Vo/3AIo?

Your reply would be much appreciated.

Best regards,
Kazuya.

  • Hi Kazuya,

    If TJ can be kept less than 125C using air or water cooling system, is it no problem to use TPS922054/5 to drive under new condition, 48Vin and  25Vo/3AIo?

    Yes. There is no problem. If designed and layout-ed well, a single TPS922054/5 can handle such amount of power output without additional heat dissipation methods like heatsink.

    Best Regards,

    Steven