This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5149: LM5149 99% Duty

Part Number: LM5149


Hi Ti,

     I want to use the function of Vout tracks Vin if the Vin is lower, whether it's mean the Pin18 PWM/SYNC can not connect to GND?  I designed a LM5149 demo-- 48V convert 24V, connected the PWM/SYNC to GND, but when I take 24V Vin, and the output voltage only is 0V.