This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650861: Schematic Review

Part Number: TPS650861

Tool/software:

Hi Team,

Please find the attached schematic for your review.

TPS65086100_Schematic_Review_TI_1.pdf

We are using PMIC (TPS65086100) in our design.   

Our design Requirement are mentioned as follows:

PMIC Regulator VIN VIN Min VIN max voltage Maximum current (peak) [A]
BUCK2 Vsys 6.6 13.2 0.734V 19.62
BUCK5 3.3V Internal 3.135 3.465 0.734V 2.025
BUCK4 3.3V Internal 3.135 3.465 0.90V 2.06
BUCK6 Vsys 6.6 13.2 1.1V 17.48
VTT_LDO BUCK6 output 1.1 1.8 0.6 (Not used) NA
BUCK1 Vsys 6.6 13.2 2.5V 16.44
BUCK3 3.3V Internal 3.135 3.465 1.8V 2.4
LDOA1 LDO5 5V 4.75 5.25 1.8V 0.08
LDO5 Vsys 6.6 13.2 5V 0.05

Kindly provide the review comments based on above design requirement. 

Thanks & Regards,

Anandraj S