Tool/software:
Hello Jeff,
Actually after continuous experimentation of the Circuit that we created with BQ25798. I observed that the output Voltage is coming 10.11V even though the prog registor is placed 17.4kohm and at VSYS I am getting 12.1V. the circuit is been designed for 4s battery charging purpose.
At PMID side, getting the same voltage as the VBUS & at REGN , I am getting the same as VBUS. Across the inductor I am getting 3.12V if the VBUS is at 5V.But as per the ideal case should be 16.8V & I am getting 10.11 V
Could you please help me out in letting me know the cause for the same. Would be great of you.
Thanks & Regards
Poorti