Other Parts Discussed in Thread: LM5145, CSD19534Q5A
Tool/software:
I've implemented the below circuit with the following specs:
1. Input voltage: 43V-58V
2. Output voltage: 24V
3. Max Current Output: 8A
When connected to a benchtop power supply with no (very small) load, I am seeing ~100mA @ 43V. Is it normal for this converter design to dissipate 4W with little to no load?