Tool/software:
Hi Jeff,
We are currently experiencing some issues with our system, which consists of a 4S battery and an 18V/5W solar panel. Specifically, we have observed the following behaviors:
- VBUS and PMID Voltage: These always reflect the voltage of the PV panel.
- SYS Voltage:
- When no battery is connected, the expected 12V for VSYSMIN is not present.
- When the battery is connected, VSYS consistently matches the battery voltage.
Additionally, we have connected the STAT pin to an LED for visual feedback. The LED is always HIGH, indicating either the batteries are charged or charging is disabled. However, we can confirm that the batteries are not charged. The /CE pin is connected to ground, assuming the EN_CHG bit is set to '1' by default.
One potential deviation from the expected setup is the prog resistor, which is 17.35k instead of the specified 17.4k for the 1.5 MHz frequency.
Could you please advise on what aspects we should focus on while debugging this behavior?
Thank you for your assistance.
Best regards,
Carlos Valente