Other Parts Discussed in Thread: UCC5390
Tool/software:
Hey TI Experts,
We are designing a circuit for Bidirectional current flow to and from a battery. The Mosfets are used in High Side Switching configuration arranged in back to back topology.
Hence, the Source terminals of both the Discharge and Charge FET are shorted.
To accomodate the above and for Isolation purpose we have an isolated supply giving 12V to the low side Gate driver and reference ground for the Source terminals.
Thus, we have the following queries:-
1) Will the FETs in high side configuration work with the low side gate driver as the Sources are shorted and always have a reference ground from the Isolated Power Supply.
2) The Isolated Power Supply is a 1:1 ratio power supply and has an output current of just 84mA. Is this sufficient for the Gate drivers current requirements.
3) Is the schematic fine interms of isolation or could be simplified/optimised more?
Would like your Valuable feedback on the same.
Thanks and Regards
Ibrahim