This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25790: OTG operation

Part Number: BQ25790


Tool/software:

Hi Team,

When OTG is working and the input is connected to Vin , what is the behavior of the device and are there any risks? Thanks!

Regards,
Hailiang

  • Hi Hailiang,

    The IC has no way to know if an adapter with voltage <= OTG-OVP threshold is plugged in.  So, it will stay in OTG mode and provide power back to the adapter.  There is little risk to the charger but not sure what the adapter will do. If the adapter cannot sink current, the VBUS pin will increase causing OVP event.  The OVP event turns off the converter and wants for the OTG output to drop to restart.  So, the input would likely have a triangular oscillation.

    Regards,

    Jeff

  • Hi Jeff,

    If the adapter cannot sink current, the VBUS pin will increase causing OVP event.
    May I know why the OVP event will occur?

    Regards,
    Hailiang

  • If Hailiang,

    When the adapter is providing a voltage and can't sink current and the charger is also providing a power at the same node, the capacitance at VBUS could overvoltage especially if charge PFM mode is disabled.  If that voltage on VBUS capacitor exceeds the threshold below, the converter turns off and reports OTG_OVP in the fault register.

    Regards,

    Jeff