This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100EVM-795: conflicting bq35100 .fs file description

Part Number: BQ35100EVM-795


Tool/software:

Hello, 

https://www.ti.com/lit/an/slua801/slua801.pdf?ts=1718397001234

section 5
describes the .df.fs file as configuration,   the .bq.fs as firmware+configuration 

This is in conflict with 

the bq35100evm description section 3.7.1:

The .srec file contains the full flash memory. The .bq.fs contains the program memory portion for the flash memory and the .df.fs contains the data flash portion of the flash memory,


What is it? 


Been running with the assumption bq.fs. is firmware. df.fs is non-firmware (config data)...though I'm not certain this assumption is correct anymore.