Tool/software:
Working with the BQ76952, I know that the TS2 Pin can be used either as a Wakeup pin or as a Thermistor ADC. I want to implement both at the same time to enable the SHUTDOWN mode which can then be waken-up through TS2 and cannot find any resources. I saw various other threads where the possibility of implementing both the functions of the TS2 is denied. Need clarity on this subject since I was thinking of designing a circuit which disconnects the TS2 and the ground when SHUTDOWN signal is given to the BQ76952 through an MCU. Will this work?