This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21710: do we need external gate pull down resistor if internal miller clamp is available

Part Number: UCC21710
Other Parts Discussed in Thread: UCC21732

Tool/software:

Hi,

I was looking at the evm and it has a 10kohm gate pull down resistor.  

Do we need external gate pull down resistor if the internal miller clamp feature is available for ucc21710?

the evm user's guide figure 2 shows the schematic for the UCC21732 (which doesn't have internal miller clamp). 

is that why you guys have R18 pull down on the evm?

please confirm whether the 10kohm R18 is required for ucc21710

-Kelvin

  • Hi Kelvin,

    Its recommended practice to plan 10Kohm gate pull down resistor (not must) so that Gate has weak pull down. It can be planned for both CLMPI or CLMPE variants.

    Thanks

    Sasi