Other Parts Discussed in Thread: BQ34Z100-G1
Tool/software:
I am looking at a 200 Amp peak and 100 Amp nominal discharge from my battery pack. And I need to use BQ34Z100-R2 which has Battery capacity (max) (MAh) 7000000 but the max input voltage is 125mV at SRN and SRP. I need to ask following two questions.
1) what should be the value of sense resistor in this case it should be 0.625mili Ohm (R=V/I is 125mV/200A) but in the previous post you recommended it should be minimum 2mili ohm for better performance.
2) If the Battery capacity (max) (MAh) 7000000 for BQ34Z100-R2 then how it is being reflected in the hardware design.
Thanks
Khalid Mahmood