This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi teams,
Currently I'm testing the TPS53689T + CSD95510 solution for customer and try to optimize the config code to let all transient margin >10mV.
And I using Nonlinear function OSR & USR to reduce over and undershoot voltage, also see the TPS53689T datasheet section 7.3.4.7 to see the OSR and USR function.
But customer tell me they don't want us using OSR and USR function because they have used other competitor controller whit similar function and cause overtemperature issue.
My questions are:
Thanks,
Vincent
Hi Vincent,
The over temperature issue what client mentioned is OSR function with Body Braking, which means the PWM will be tri-state and the continuous inductor current will go through body diode of low side MOS after trigger OSR function. That will be the temperature rising because of the large free wheeling current from inductor x Vdiode.
We do recommend that enable OSR function without Body Braking.
For both OSR and USR functions, please refer to the 7.3.4.7 Nonlinear: Undershoot Reduction (USR), Overshoot Reduction (OSR) and Dynamic Integration in datasheet.
Best regards,
Jack Su