Tool/software:
I having an issue I have is that I successfully set the Design Capacity and Design Energy to 7000 mAh and 7560 MWh under Data Memory but when viewing the gauges Registers its showing Full Charge and Remaining Charge of 3262. My expectation here would be that this value would approximately mirror the Design Capacity value of 7000. What parameter do I need to set to get this value correct? I also attempted to change the Qmax Cell 0 parameter under Data Memory Gas Gauging to 7000 but that did not change this value either. How do I get this parameter to properly represent the battery pack capacity? BQ34Z100PWR-G1 Gauge Configuration Issue.docx
Will this only get adjusted during the learning cycle? Please assist.