This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561: BQ25185DLHR LOW CURRENT CHARGING

Part Number: BQ27Z561


Tool/software:

Hello,

I have an inr18650-35E 4p battery pack, a bq27z561 gauge, and a BQ25185DLHR charger. We're charging this battery off of solar...And the charge current is very low-Around 50mA. Cutoff of the pack is 272mA and currently the charger cutoff is configured for 30mA.

How do I determine end of charge given such a low current. Traditional graphs of the CC/CV plot, the constant current is much greater than this, So you can reach you CV (constant Voltage) phased and then just monitor until cutoff current is reached or time expires. 

How do I do this in the current configuration? How do I compute the time required to charge once reaching CV phase?

Additionally how do I set the term taper current, given the charger cutoff current is LOWER than the battery pack cutoff?

  • Hello Craig, 

    Can you please clarify what you are referring to with the battery pack cutoff and the charger cutoff? It sounds like the charger cutoff is the current that the charge tapers down to before cutting off, is this correct? 

    Regards, 

    Jonny. 

  • sure. I'm looking at the inr18650-35E data sheet. It specifies a standard charge (constant current/constant voltage), of 1700mA (constnat current mode), 4.2V (constant voltage mode), that dwindles to 68mA cutoff current to achieve rated capacity of 3400mAh. We have a 4p pack so 4*68mA = 272mA cutoff for the pack.

    Currently our charger cutoff (when the charger stops providing current) is 30mA. Solar currents are expected around 50mA. 

    30mA is well below the battery cutoff current...Thus this charger isn't really operating like one would expect where it's usually expeceted that charger current cutoff is at or above the pack cutoff. 

    Basically 'current' is not how we'll detect a full charge with the charger-Is that how the gauge alogrithm works? It determines charge purely on current?

    We might/probably have to do some manual control of the charger to preclude overcharging. 

    What should I use for the term charge taper current? Is it possible to run the learning calibration assuming a standard charger, and then use that image in the solar charge setup (would it still gauge accuratetly?).

    Will this gauge work with our current setup?



  • Hey Craig, 

    Thank you for the clarification. I don't believe that this should be an issue, it looks like the battery datasheet is saying the typical battery charge taper rate is 68mA. You should be able to set the taper current on the gauge to be about 10% higher than the cutoff current for the charger, so 35mA. You should just ensure that the chg threshold current is less than the 30mA so that the gauge detects a charge even when in the taper phase of the charging. 

    Regards, 

    Jonny. 

  • Thanks, Jonny.

    Here I was asking a similar question here:

    BQ27Z561: bq27z561 learning cycle question - Power management forum - Power management - TI E2E support forums


    I guess my question is the charge term taper current, will not really indicate end of charge in our setup. Our charge will always be supply less than battery cutoff so it's not a good marker for FULL charge. Is the taper current used to indicated FULL charge?

    We'll have to manually verify end of charge by other means (shutdown the charge process in software monitoring voltage, or setting a timer....TBD).

    Is the gauge smart of enough to track charge for the little current that is injected to it OR will it see a low current and say FULL charge when its actually just in the middle of of charge? - THAT IS MY CONCERN.

    This is the IT algorithm doc:
    Evaluation 3: Theory/Implementation Impedance Track Battery Fuel-Gauging Algo (R ev. B

    From there:

    DODcharge is assigned equal to DOD0 aft first DOD0 update after CHARGE TERMINATION BY TAPER CURRENT

    where 

    Qstart = Qmax (DOD0 - DODcharge)

    Thus Qstart would equal ZERO and thus be equivalent to a full charge? 


    I'm concerned that the taper current is being used to determine FULL CHARGE


    Additionally. Our application has an active state and sleep state with current ranges from 1.8A during message transmission, averaging  maybe 500mA and hopefully sub-milliamp (microamp) current levels during sleep. The sub=milliamp is hopeful/optimized levels we have NOT reached yet. Are realistic current discharge is probably a couple milliamps

    Will the gauge work accurately given the low current draw?

    What DSG Current Threshold should be used given our application-Should it be based off the wake state?



    I'm not an expert in the alogrithm. Most of my time spent on the driver was implementing the calibration procedures on a microcontroller and working through errors in the documentation. 

     

    From a battery perspective (not an expert), the end of charge is determined by 4.2V being reached (Constant voltage mode entered) and the current dwindling decreasing from a current higher than cutoff current (say 1700mA), down to the cutoff current. 

     

    We can't track this decrease as our solar charge current is at best 50ma (always below BATTERY cutoff) and thus cannot use this for determining charge. To me, the IT alogrithm indicates taper current (perecursor to cutoff current) is utilized in indicating full charge

     

    IF the gauge is using current level as the determining factor to indicate FULL CHARGE then i fear it could indicate full charge when it's actually not. OR the gauge doesn't work for our setup.

     

    I feel the gauge would work fine with a standard charger (High charge current in CC phase that dwindle to cutoff current in CV phase)...but our current setup is suspect to me.

    So three 'cutoff currents at play'

     

    CHARGER cutoff current -    30mA

     

    GAUGE Assigned taper current (related to the cutoff current of charger), set by us but deduced from charger...say 35 mA

     

    BATTERY cutoff current  at standard charge 1700mA CC mode, 4.2V CV mode, 68mA for a cell--->272mA for the 4p pack

    I'm not certain these are aligned-hence I'm concerned about hw (charger->gauge->battery) compatibility



    Thanks!

  • Hello,

    Today's a national holiday. We will get back to you tomorrow.

    Regards,

    TI Apps Team

  • Hello Craig, 

    Please refer to section 9.8 Valid Charge Termination from the BQ27z561 TRM. The gauge uses the taper rate along with a couple of other parameters to report SOC 100%. If the taper rate condition is not met, then the gauge will not report 100%. 

    Regards, 

    Jonny.