This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Chem ID Characterization

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: GPCCHEM

Tool/software:

I am running into the same problem after using the GPCChem tool and SLVA725A procedure. My best chem id deviation is 12.11%. I am using a battery pack with 8 series (3.2V and 4Ah) LiFePo4 cells. I believe this battery pack needs to be characterized unless you want to look at the data first. I can send over 3 rechargeable battery packs and any battery information needed such as battery datasheet, GPC_report, log data, and cell characterization form. I will also need a FAE contact to receive a quote.

Thank you,

Cole