This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi
customer search for an DCDC with adj current limit similar to LM5015.
Vin: 4,25V to 75V
Iout: 1A to 3A
adj current limit
two switch forward with galv. iso
Regards, Holger
Hi Youhao,
a solution with an external FET is also accepted.
Regards, Holger
Youhao,
You can find the device that fits your specifications here. Once you select the topology desired, you can filter by features and select Adjustable current limit. Same for the other parameters.
Thank you
Hi Manuel,
Thank you but I just don't know which one is suitable. We are in the WVB product line and we are not familiar with the isolated power except for the flyback. We do have LM518x to implement a PSR flyback to produce isolated output, but they do not have adj current limit nor it support two switch forward.
Note that the thread has LM5015 in the subject line so it came to our attention. However, our product line do not have a part to meet the requirement. The LM5015 is a two switch forward converter but it does not have adj current limit either. This is why I forward it to HVC's attention, hoping they may have something to support. Let's wait for their comments.
Regards,
Youhao