This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23881: Port 1 power is low

Part Number: TPS23881


Tool/software:

This is the circuit diagram of TPS23881 in the attachment. The four ports controlled by TPS23881, port 1 is protected at 95W, while the other three ports are protected at 110W. How to increase port 1 to 110W for protection? Please provide relevant solutions and methods. The maximum output power has been set to 0xff, and the input voltage of the circuit is 55v.

PSE_4M_TPS23881.PDF