This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2660: TPS26601 OVP & UVLO FAULT TRIGGERING NOT FUCNTIONING IN STARTUP BEHAVIOUR PSPICE SIMULATION

Part Number: TPS2660

Tool/software:

I tried simulating TPS26601 Transient Model in Start Up state. I see difference in behavior of simulation output vs calculated results.

Calculated Values of R1,R2, & R3 for OVP & UVLO fault as per TI Spreadsheet calculator as below,

I used the same recommended values of R1,R2 &R3 in pspice simulation shown below,

As per calculated threshold limits shown in above spreadsheet calculation, Fault is not triggering at 3.4%.

Simulation observation :

UVLO Fault triggering at 44.71V

OVP Fault triggering at 48.8V

Could you please clarify it & pspice model i download is write access denied - it could be problem in getting wrong outputs?

Thanks

Dharma