This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi ,
iam workng on bq25622 battery charger .
my battery current showing zero.
Please tell me the settings for battery current .
Kindly help me on this.
Thanks,
Naresh
Hi Ning,
Yes, battery current showing Zero amperes.
Could you please help me with the register configurations?
Please help me driver changes if any.
Or else give me latest bq25622 latest driver.
Please help, which is critical for us
My mail id is naresh.nakka@tessolve.com
Thanks,
Naresh.
HI Ning ,
Thanks for attatching driver .
I am attaching my changes in the driver , which makes me charging , discarging and charging full showing bu i observed below issue.
letsay ,when i read the statuus charging , and battery current showing 2mA , after 10 min also showing same . if i reboot /power cycle only chagnes are reflecting ,
Kindly help me on this . its urgent.
my changes are done with name comment name "TESSOLVE" in driver .
// SPDX-License-Identifier: GPL-2.0 // BQ2562X driver // Copyright (C) 2020 Texas Instruments Incorporated - http://www.ti.com/ #include <linux/module.h> #include <linux/i2c.h> #include <linux/power_supply.h> #include <linux/regmap.h> #include <linux/types.h> #include <linux/gpio/consumer.h> #include <linux/interrupt.h> #include <linux/delay.h> #include <linux/usb/phy.h> #include <linux/acpi.h> #include <linux/of.h> #include <linux/gpio.h> #include <linux/of_gpio.h> #include "bq2562x_charger.h" #define BQ2562X_NUM_WD_VAL 4 int gpio_num; struct bq2562x_init_data { u32 ichg; u32 ilim; u32 vreg; u32 iterm; u32 iprechg; u32 vlim; u32 ichg_max; u32 vreg_max; }; struct bq2562x_state { bool online; u8 chrg_status; u8 chrg_type; u8 health; u8 chrg_fault; u8 vsys_status; u8 vbus_status; u8 fault_0; u8 fault_1; u32 vbat_adc; u32 vbus_adc; u32 ibat_adc; u32 ibus_adc; }; enum bq2562x_id { BQ25620, BQ25622, }; struct bq2562x_device { struct i2c_client *client; struct device *dev; struct power_supply *charger; struct power_supply *battery; struct mutex lock; struct usb_phy *usb2_phy; struct usb_phy *usb3_phy; struct notifier_block usb_nb; struct work_struct usb_work; unsigned long usb_event; struct regmap *regmap; char model_name[I2C_NAME_SIZE]; int device_id; struct gpio_desc *ac_detect_gpio; struct gpio_desc *ce_gpio; struct bq2562x_init_data init_data; struct bq2562x_state state; int watchdog_timer; }; static struct reg_default bq25620_reg_defs[] = { {BQ2562X_CHRG_I_LIM_MSB, 0x03}, {BQ2562X_CHRG_I_LIM_LSB, 0x40}, {BQ2562X_CHRG_V_LIM_MSB, 0x0D}, {BQ2562X_CHRG_V_LIM_LSB, 0x20}, {BQ2562X_INPUT_I_LIM_MSB, 0x0A}, {BQ2562X_INPUT_I_LIM_LSB, 0x00}, {BQ2562X_INPUT_V_LIM_MSB, 0x0E}, {BQ2562X_INPUT_V_LIM_LSB, 0x60}, {BQ2562X_IOTG_MSB, 0x03}, {BQ2562X_IOTG_LSB, 0x20}, {BQ2562X_VOTG_MSB, 0x0F}, {BQ2562X_VOTG_LSB, 0xC0}, {BQ2562X_MIN_SYS_V_MSB, 0x0B}, {BQ2562X_MIN_SYS_V_LSB, 0x00}, {BQ2562X_PRECHRG_CTRL_MSB, 0x00}, {BQ2562X_PRECHRG_CTRL_LSB, 0x50}, {BQ2562X_TERM_CTRL_MSB, 0x00}, {BQ2562X_TERM_CTRL_LSB, 0x30}, {BQ2562X_CHRG_CTRL, 0x06}, {BQ2562X_TIMER_CTRL, 0x5C}, {BQ2562X_CHRG_CTRL_0, 0xA1}, {BQ2562X_CHRG_CTRL_1, 0x4E}, {BQ2562X_CHRG_CTRL_2, 0x04}, {BQ2562X_CHRG_CTRL_3, 0xC4}, {BQ2562X_NTC_CTRL_0, 0x3D}, {BQ2562X_NTC_CTRL_1, 0x25}, {BQ2562X_NTC_CTRL_2, 0x3F}, {BQ2562X_CHRG_STAT_0, 0x00}, {BQ2562X_CHRG_STAT_1, 0x00}, {BQ2562X_FAULT_STAT_0, 0x00}, {BQ2562X_CHRG_FLAG_0, 0x00}, {BQ2562X_CHRG_FLAG_1, 0x00}, {BQ2562X_FAULT_FLAG_0, 0x00}, {BQ2562X_CHRG_MSK_0, 0x00}, {BQ2562X_CHRG_MSK_1, 0x00}, {BQ2562X_FAULT_MSK_0, 0x00}, {BQ2562X_ADC_CTRL, 0x30}, {BQ2562X_FN_DISABE_0, 0x00}, {BQ2562X_ADC_IBUS_MSB, 0x00}, {BQ2562X_ADC_IBUS_LSB, 0x00}, {BQ2562X_ADC_IBAT_MSB, 0x00}, {BQ2562X_ADC_IBAT_LSB, 0x00}, {BQ2562X_ADC_VBUS_MSB, 0x00}, {BQ2562X_ADC_VBUS_LSB, 0x00}, {BQ2562X_ADC_VPMID_MSB, 0x00}, {BQ2562X_ADC_VPMID_LSB, 0x00}, {BQ2562X_ADC_VBAT_MSB, 0x00}, {BQ2562X_ADC_VBAT_LSB, 0x00}, {BQ2562X_ADC_VSYS_MSB, 0x00}, {BQ2562X_ADC_VSYS_LSB, 0x00}, {BQ2562X_ADC_TS_MSB, 0x00}, {BQ2562X_ADC_TS_LSB, 0x00}, {BQ2562X_ADC_TDIE_MSB, 0x00}, {BQ2562X_ADC_TDIE_LSB, 0x00}, {BQ2562X_PART_INFO, 0x00}, }; static struct reg_default bq25622_reg_defs[] = { {BQ2562X_CHRG_I_LIM_MSB, 0x03}, {BQ2562X_CHRG_I_LIM_LSB, 0x40}, {BQ2562X_CHRG_V_LIM_MSB, 0x0D}, {BQ2562X_CHRG_V_LIM_LSB, 0x20}, {BQ2562X_INPUT_I_LIM_MSB, 0x0A}, {BQ2562X_INPUT_I_LIM_LSB, 0x00}, {BQ2562X_INPUT_V_LIM_MSB, 0x0E}, {BQ2562X_INPUT_V_LIM_LSB, 0x60}, {BQ2562X_IOTG_MSB, 0x03}, {BQ2562X_IOTG_LSB, 0x20}, {BQ2562X_VOTG_MSB, 0x0F}, {BQ2562X_VOTG_LSB, 0xC0}, {BQ2562X_MIN_SYS_V_MSB, 0x0B}, {BQ2562X_MIN_SYS_V_LSB, 0x00}, {BQ2562X_PRECHRG_CTRL_MSB, 0x00}, {BQ2562X_PRECHRG_CTRL_LSB, 0x50}, {BQ2562X_TERM_CTRL_MSB, 0x00}, {BQ2562X_TERM_CTRL_LSB, 0x30}, {BQ2562X_CHRG_CTRL, 0x06}, {BQ2562X_TIMER_CTRL, 0x5C}, {BQ2562X_CHRG_CTRL_0, 0xA1}, {BQ2562X_CHRG_CTRL_1, 0x4E}, {BQ2562X_CHRG_CTRL_2, 0x04}, {BQ2562X_CHRG_CTRL_3, 0xC4}, {BQ2562X_NTC_CTRL_0, 0x3D}, {BQ2562X_NTC_CTRL_1, 0x25}, {BQ2562X_NTC_CTRL_2, 0x3F}, {BQ2562X_CHRG_STAT_0, 0x00}, {BQ2562X_CHRG_STAT_1, 0x00}, {BQ2562X_FAULT_STAT_0, 0x00}, {BQ2562X_CHRG_FLAG_0, 0x00}, {BQ2562X_CHRG_FLAG_1, 0x00}, {BQ2562X_FAULT_FLAG_0, 0x00}, {BQ2562X_CHRG_MSK_0, 0x00}, {BQ2562X_CHRG_MSK_1, 0x00}, {BQ2562X_FAULT_MSK_0, 0x00}, {BQ2562X_ADC_CTRL, 0x30}, {BQ2562X_FN_DISABE_0, 0x00}, {BQ2562X_ADC_IBUS_MSB, 0x00}, {BQ2562X_ADC_IBUS_LSB, 0x00}, {BQ2562X_ADC_IBAT_MSB, 0x00}, {BQ2562X_ADC_IBAT_LSB, 0x00}, {BQ2562X_ADC_VBUS_MSB, 0x00}, {BQ2562X_ADC_VBUS_LSB, 0x00}, {BQ2562X_ADC_VPMID_MSB, 0x00}, {BQ2562X_ADC_VPMID_LSB, 0x00}, {BQ2562X_ADC_VBAT_MSB, 0x00}, {BQ2562X_ADC_VBAT_LSB, 0x00}, {BQ2562X_ADC_VSYS_MSB, 0x00}, {BQ2562X_ADC_VSYS_LSB, 0x00}, {BQ2562X_ADC_TS_MSB, 0x00}, {BQ2562X_ADC_TS_LSB, 0x00}, {BQ2562X_ADC_TDIE_MSB, 0x00}, {BQ2562X_ADC_TDIE_LSB, 0x00}, {BQ2562X_PART_INFO, 0x00}, }; static int bq2562x_watchdog_time[BQ2562X_NUM_WD_VAL] = {0, 40000, 80000, 160000}; static enum power_supply_usb_type bq2562x_usb_type[] = { POWER_SUPPLY_USB_TYPE_ACA, POWER_SUPPLY_USB_TYPE_SDP, POWER_SUPPLY_USB_TYPE_CDP, POWER_SUPPLY_USB_TYPE_DCP, POWER_SUPPLY_USB_TYPE_UNKNOWN, }; static int bq2562x_usb_notifier(struct notifier_block *nb, unsigned long val, void *priv) { struct bq2562x_device *bq = container_of(nb, struct bq2562x_device, usb_nb); bq->usb_event = val; queue_work(system_power_efficient_wq, &bq->usb_work); return NOTIFY_OK; } static void bq2562x_usb_work(struct work_struct *data) { struct bq2562x_device *bq = container_of(data, struct bq2562x_device, usb_work); switch (bq->usb_event) { case USB_EVENT_ID: break; case USB_EVENT_NONE: power_supply_changed(bq->charger); break; } } static bool bq2562x_get_charge_enable(struct bq2562x_device *bq) { int ret; int ce_pin; int charger_enable; int chrg_ctrl_0; if (bq->ce_gpio) ce_pin = gpiod_get_value_cansleep(bq->ce_gpio); ret = gpio_direction_output(gpio_num, 0); //TESSOLVE ret = regmap_read(bq->regmap, BQ2562X_CHRG_CTRL_0, &chrg_ctrl_0); if (ret) return ret; charger_enable = chrg_ctrl_0 & BQ2562X_CHRG_EN; if (charger_enable) { if (bq->ce_gpio && !ce_pin) return true; } //return false; return true; //TESSOLVE } static int bq2562x_set_charge_enable(struct bq2562x_device *bq, int val) { gpiod_set_value_cansleep(bq->ce_gpio, !val); //gpio_direction_output(gpio_num, !val); //TESSOLVE return regmap_update_bits(bq->regmap, BQ2562X_CHRG_CTRL_0, BQ2562X_CHRG_EN, val); } static int bq2562x_get_vbat_adc(struct bq2562x_device *bq) { int ret; int vbat_adc_lsb, vbat_adc_msb; u16 vbat_adc; ret = regmap_read(bq->regmap, BQ2562X_ADC_VBAT_LSB, &vbat_adc_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_ADC_VBAT_MSB, &vbat_adc_msb); if (ret) return ret; vbat_adc = ((vbat_adc_msb << 8) | vbat_adc_lsb) >> BQ2562X_ADC_VBAT_MOVE_STEP; return vbat_adc * BQ2562X_ADC_VBAT_STEP_uV; } static int bq2562x_get_vbus_adc(struct bq2562x_device *bq) { int ret; int vbus_adc_lsb, vbus_adc_msb; u16 vbus_adc; ret = regmap_read(bq->regmap, BQ2562X_ADC_VBUS_LSB, &vbus_adc_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_ADC_VBUS_MSB, &vbus_adc_msb); if (ret) return ret; vbus_adc = ((vbus_adc_msb << 8) | vbus_adc_lsb) >> BQ2562X_ADC_VBUS_MOVE_STEP; return vbus_adc * BQ2562X_ADC_VBUS_STEP_uV; } static int bq2562x_get_ibat_adc(struct bq2562x_device *bq) { int ret; int ibat_adc_lsb, ibat_adc_msb; u16 ibat_adc; ret = regmap_read(bq->regmap, BQ2562X_ADC_IBAT_LSB, &ibat_adc_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_ADC_IBAT_MSB, &ibat_adc_msb); if (ret) return ret; ibat_adc = ((ibat_adc_msb << 8) | ibat_adc_lsb) >> BQ2562X_ADC_IBAT_MOVE_STEP; return ibat_adc * BQ2562X_ADC_IBAT_STEP_uV; } static int bq2562x_get_ibus_adc(struct bq2562x_device *bq) { int ret; int ibus_adc_lsb, ibus_adc_msb; int ibus_adc; ret = regmap_read(bq->regmap, BQ2562X_ADC_IBUS_LSB, &ibus_adc_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_ADC_IBUS_MSB, &ibus_adc_msb); if (ret) return ret; ibus_adc = ((ibus_adc_msb << 8) | ibus_adc_lsb) >> BQ2562X_ADC_IBUS_MOVE_STEP; return ibus_adc * BQ2562X_ADC_CURR_STEP_uA; } static int bq2562x_get_term_curr(struct bq2562x_device *bq) { int ret; int iterm_lsb, iterm_msb; u16 iterm; ret = regmap_read(bq->regmap, BQ2562X_TERM_CTRL_LSB, &iterm_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_TERM_CTRL_MSB, &iterm_msb); if (ret) return ret; iterm = ((iterm_msb << 8) | iterm_lsb) >> BQ2562X_ITERM_MOVE_STEP; return iterm * BQ2562X_TERMCHRG_CURRENT_STEP_uA; } static int bq2562x_get_prechrg_curr(struct bq2562x_device *bq) { int ret; int prechrg_curr_lsb, prechrg_curr_msb; u16 prechrg_curr; ret = regmap_read(bq->regmap, BQ2562X_PRECHRG_CTRL_LSB, &prechrg_curr_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_PRECHRG_CTRL_MSB, &prechrg_curr_msb); if (ret) return ret; prechrg_curr = ((prechrg_curr_msb << 8) | prechrg_curr_lsb) >> BQ2562X_PRECHRG_MOVE_STEP; return prechrg_curr * BQ2562X_PRECHRG_CURRENT_STEP_uA; } static int bq2562x_get_ichg_curr(struct bq2562x_device *bq) { int ret; int ichg, ichg_lsb, ichg_msb; ret = regmap_read(bq->regmap, BQ2562X_CHRG_I_LIM_MSB, &ichg_msb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_CHRG_I_LIM_LSB, &ichg_lsb); if (ret) return ret; ichg = ((ichg_msb << 8) | ichg_lsb) >> BQ2562X_ICHG_MOVE_STEP; return ichg * BQ2562X_ICHRG_CURRENT_STEP_uA; } static int bq2562x_set_term_curr(struct bq2562x_device *bq, int term_current) { int reg_val; int term_curr_msb, term_curr_lsb; int ret; term_current = clamp(term_current, BQ2562X_TERMCHRG_I_MIN_uA, BQ2562X_TERMCHRG_I_MAX_uA); reg_val = (term_current / BQ2562X_TERMCHRG_CURRENT_STEP_uA) << BQ2562X_ITERM_MOVE_STEP; term_curr_msb = (reg_val >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_TERM_CTRL_MSB, term_curr_msb); if (ret) return ret; term_curr_lsb = reg_val & 0xff; return regmap_write(bq->regmap, BQ2562X_TERM_CTRL_LSB, term_curr_lsb); } static int bq2562x_set_prechrg_curr(struct bq2562x_device *bq, int pre_current) { int reg_val; int prechrg_curr_msb, prechrg_curr_lsb; int ret; pre_current = clamp(pre_current, BQ2562X_PRECHRG_I_MIN_uA, BQ2562X_PRECHRG_I_MAX_uA); bq2562x_set_charge_enable(bq, 0); reg_val = (pre_current / BQ2562X_PRECHRG_CURRENT_STEP_uA) << BQ2562X_PRECHRG_MOVE_STEP; prechrg_curr_msb = (reg_val >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_PRECHRG_CTRL_MSB, prechrg_curr_msb); if (ret) return ret; prechrg_curr_lsb = reg_val & 0xff; ret = regmap_write(bq->regmap, BQ2562X_PRECHRG_CTRL_LSB, prechrg_curr_lsb); if (ret) return ret; return bq2562x_set_charge_enable(bq, 1); } static int bq2562x_set_ichrg_curr(struct bq2562x_device *bq, int chrg_curr) { int chrg_curr_max = bq->init_data.ichg_max; int ichg, ichg_msb, ichg_lsb; int ret; chrg_curr = clamp(chrg_curr, BQ2562X_ICHRG_I_MIN_uA, chrg_curr_max); bq2562x_set_charge_enable(bq, 0); ichg = ((chrg_curr / BQ2562X_ICHRG_CURRENT_STEP_uA) << BQ2562X_ICHG_MOVE_STEP); ichg_msb = (ichg >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_CHRG_I_LIM_MSB, ichg_msb); if (ret) return ret; ichg_lsb = ichg & 0xff; ret = regmap_write(bq->regmap, BQ2562X_CHRG_I_LIM_LSB, ichg_lsb); if (ret) return ret; return bq2562x_set_charge_enable(bq, 1); } static int bq2562x_set_chrg_volt(struct bq2562x_device *bq, int chrg_volt) { int chrg_volt_max = bq->init_data.vreg_max; int chrg_volt_lsb, chrg_volt_msb, vlim; int ret; chrg_volt = clamp(chrg_volt, BQ2562X_VREG_V_MIN_uV, chrg_volt_max); vlim = (chrg_volt / BQ2562X_VREG_V_STEP_uV) << BQ2562X_CHRG_V_LIM_MOVE_STEP; chrg_volt_msb = (vlim >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_CHRG_V_LIM_MSB, chrg_volt_msb); if (ret) return ret; chrg_volt_lsb = vlim & 0xff; return regmap_write(bq->regmap, BQ2562X_CHRG_V_LIM_LSB, chrg_volt_lsb); } static int bq2562x_get_chrg_volt(struct bq2562x_device *bq) { int ret; int chrg_volt_lsb, chrg_volt_msb, chrg_volt; ret = regmap_read(bq->regmap, BQ2562X_CHRG_V_LIM_LSB, &chrg_volt_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_CHRG_V_LIM_MSB, &chrg_volt_msb); if (ret) return ret; chrg_volt = ((chrg_volt_msb << 8) | chrg_volt_lsb) >> BQ2562X_CHRG_V_LIM_MOVE_STEP; return chrg_volt * BQ2562X_VREG_V_STEP_uV; } static int bq2562x_set_input_volt_lim(struct bq2562x_device *bq, int vindpm) { int ret; int vlim_lsb, vlim_msb; int vlim; vindpm = clamp(vindpm, BQ2562X_VINDPM_V_MIN_uV, BQ2562X_VINDPM_V_MAX_uV); vlim = (vindpm / BQ2562X_VINDPM_STEP_uV) << BQ2562X_INPUT_V_LIM_MOVE_STEP; vlim_msb = (vlim >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_INPUT_V_LIM_MSB, vlim_msb); if (ret) return ret; vlim_lsb = vlim & 0xff; return regmap_write(bq->regmap, BQ2562X_INPUT_V_LIM_LSB, vlim_lsb); } static int bq2562x_get_input_volt_lim(struct bq2562x_device *bq) { int ret; int vlim; int vlim_lsb, vlim_msb; ret = regmap_read(bq->regmap, BQ2562X_INPUT_V_LIM_LSB, &vlim_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_INPUT_V_LIM_MSB, &vlim_msb); if (ret) return ret; vlim = ((vlim_msb << 8) | vlim_lsb) >> BQ2562X_INPUT_V_LIM_MOVE_STEP; return vlim * BQ2562X_VINDPM_STEP_uV; } static int bq2562x_set_input_curr_lim(struct bq2562x_device *bq, int iindpm) { int ret; int ilim, ilim_lsb, ilim_msb; iindpm = clamp(iindpm, BQ2562X_IINDPM_I_MIN_uA, BQ2562X_IINDPM_I_MAX_uA); ilim = (iindpm / BQ2562X_IINDPM_STEP_uA) << BQ2562X_INPUT_I_LIM__MOVE_STEP; ilim_lsb = ilim & 0xff; ret = regmap_write(bq->regmap, BQ2562X_INPUT_I_LIM_LSB, ilim_lsb); if (ret) return ret; ilim_msb = (ilim >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_INPUT_I_LIM_MSB, ilim_msb); return ret; } static int bq2562x_get_input_curr_lim(struct bq2562x_device *bq) { int ret; int ilim_msb, ilim_lsb; u16 ilim; ret = regmap_read(bq->regmap, BQ2562X_INPUT_I_LIM_LSB, &ilim_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_INPUT_I_LIM_MSB, &ilim_msb); if (ret) return ret; ilim = ((ilim_msb << 8) | ilim_lsb) >> BQ2562X_INPUT_I_LIM__MOVE_STEP; return ilim * BQ2562X_IINDPM_STEP_uA; } static int bq2562x_get_online_status(struct bq2562x_device *bq) { int ret; int chrg_stat_1; int online_status; ret = regmap_update_bits(bq->regmap, BQ2562X_CHRG_STAT_1, BQ2562X_VBUS_STAT_MSK, BQ2562X_UNKNOWN_500MA); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_CHRG_STAT_1, &chrg_stat_1); if (ret) return ret; online_status = chrg_stat_1 & BQ2562X_VBUS_STAT_MSK; if ((online_status == BQ2562X_USB_SDP) || (online_status == BQ2562X_OTG_MODE)) online_status = 0; else online_status = 1; return online_status; } static int bq2562x_get_state(struct bq2562x_device *bq, struct bq2562x_state *state) { int chrg_stat_0, chrg_stat_1; int fault_0, fault_1; int ret; int val = 0; ret = regmap_update_bits(bq->regmap, BQ2562X_ADC_CTRL, BQ2562X_ADC_EN, BQ2562X_ADC_EN); if (ret) return ret; if (bq->ac_detect_gpio) { val = gpiod_get_value_cansleep(bq->ac_detect_gpio); state->vbus_status = val; } ret = regmap_read(bq->regmap, BQ2562X_CHRG_STAT_1, &chrg_stat_1); if (ret) return ret; if (bq2562x_get_charge_enable(bq)) state->chrg_status = chrg_stat_1 & BQ2562X_CHG_STAT_MSK; else state->chrg_status = BQ2562X_NOT_CHRGING; state->chrg_type = chrg_stat_1 & BQ2562X_VBUS_STAT_MSK; ret = regmap_read(bq->regmap, BQ2562X_FAULT_STAT_0, &fault_0); if (ret) return ret; state->health = fault_0 & BQ2562X_TEMP_MASK; state->fault_0 = fault_0; ret = regmap_read(bq->regmap, BQ2562X_FAULT_STAT_0, &fault_1); if (ret) return ret; state->fault_1 = fault_1; ret = regmap_read(bq->regmap, BQ2562X_CHRG_STAT_0, &chrg_stat_0); if (ret) return ret; state->online = bq2562x_get_online_status(bq); state->vbat_adc = bq2562x_get_vbat_adc(bq); state->vbus_adc = bq2562x_get_vbus_adc(bq); state->ibat_adc = bq2562x_get_ibat_adc(bq); state->ibus_adc = bq2562x_get_ibus_adc(bq); return 0; } static void bq2562x_charger_reset(void *data) { struct bq2562x_device *bq = data; if (!IS_ERR_OR_NULL(bq->usb2_phy)) usb_unregister_notifier(bq->usb2_phy, &bq->usb_nb); if (!IS_ERR_OR_NULL(bq->usb3_phy)) usb_unregister_notifier(bq->usb3_phy, &bq->usb_nb); } static int bq2562x_set_property(struct power_supply *psy, enum power_supply_property prop, const union power_supply_propval *val) { struct bq2562x_device *bq = power_supply_get_drvdata(psy); int ret = -EINVAL; switch (prop) { case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT: ret = bq2562x_set_input_curr_lim(bq, val->intval); break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE: ret = bq2562x_set_chrg_volt(bq, val->intval); break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT: ret = bq2562x_set_ichrg_curr(bq, val->intval); break; case POWER_SUPPLY_PROP_PRECHARGE_CURRENT: ret = bq2562x_set_prechrg_curr(bq, val->intval); break; case POWER_SUPPLY_PROP_CHARGE_TERM_CURRENT: ret = bq2562x_set_term_curr(bq, val->intval); break; case POWER_SUPPLY_PROP_INPUT_VOLTAGE_LIMIT: ret = bq2562x_set_input_volt_lim(bq, val->intval); break; default: return -EINVAL; } return ret; } static int bq2562x_get_property(struct power_supply *psy, enum power_supply_property psp, union power_supply_propval *val) { struct bq2562x_device *bq = power_supply_get_drvdata(psy); struct bq2562x_state state; int ret = 0; ret = bq2562x_get_state(bq, &state); if (ret) return ret; switch (psp) { case POWER_SUPPLY_PROP_STATUS: if (!state.chrg_type || (state.chrg_type == BQ2562X_OTG_MODE)) val->intval = POWER_SUPPLY_STATUS_DISCHARGING; else if (!state.chrg_status) { val->intval = POWER_SUPPLY_STATUS_NOT_CHARGING; if (bq2562x_get_chrg_volt(bq) >= (state.vbat_adc - BQ2562X_ADC_VBAT_STEP_uV)) val->intval = POWER_SUPPLY_STATUS_FULL; } //else if (state.chrg_status == BQ2562X_TERM_CHRG) // val->intval = POWER_SUPPLY_STATUS_FULL; else val->intval = POWER_SUPPLY_STATUS_CHARGING; break; case POWER_SUPPLY_PROP_CHARGE_TYPE: switch (state.chrg_status) { case BQ2562X_TRICKLE_CHRG: val->intval = POWER_SUPPLY_CHARGE_TYPE_TRICKLE; break; case BQ2562X_TAPER_CHRG: val->intval = POWER_SUPPLY_CHARGE_TYPE_STANDARD; break; case BQ2562X_TOP_OFF_CHRG: val->intval = POWER_SUPPLY_CHARGE_TYPE_TRICKLE; break; case BQ2562X_NOT_CHRGING: val->intval = POWER_SUPPLY_CHARGE_TYPE_NONE; break; default: val->intval = POWER_SUPPLY_CHARGE_TYPE_UNKNOWN; } break; case POWER_SUPPLY_PROP_MANUFACTURER: val->strval = BQ2562X_MANUFACTURER; break; case POWER_SUPPLY_PROP_MODEL_NAME: val->strval = bq->model_name; break; case POWER_SUPPLY_PROP_ONLINE: val->intval = state.online; break; case POWER_SUPPLY_PROP_USB_TYPE: if (!state.chrg_type) { val->intval = POWER_SUPPLY_USB_TYPE_UNKNOWN; break; } switch (state.chrg_type) { case BQ2562X_USB_SDP: val->intval = POWER_SUPPLY_USB_TYPE_SDP; break; case BQ2562X_USB_CDP: val->intval = POWER_SUPPLY_USB_TYPE_CDP; break; case BQ2562X_USB_DCP: val->intval = POWER_SUPPLY_USB_TYPE_DCP; break; case BQ2562X_OTG_MODE: val->intval = POWER_SUPPLY_USB_TYPE_ACA; break; default: val->intval = POWER_SUPPLY_USB_TYPE_UNKNOWN; break; } break; case POWER_SUPPLY_PROP_HEALTH: if (state.fault_1 & (BQ2562X_OTG_FAULT_STAT | BQ2562X_SYS_FAULT_STAT)) val->intval = POWER_SUPPLY_HEALTH_OVERVOLTAGE; else val->intval = POWER_SUPPLY_HEALTH_GOOD; switch (state.health) { case BQ2562X_TEMP_TS_NORMAL: val->intval = POWER_SUPPLY_HEALTH_GOOD; break; case BQ2562X_TEMP_HOT: val->intval = POWER_SUPPLY_HEALTH_HOT; break; case BQ2562X_TEMP_WARM: case BQ2562X_TEMP_PREWARM: val->intval = POWER_SUPPLY_HEALTH_WARM; break; case BQ2562X_TEMP_COOL: case BQ2562X_TEMP_PRECOOL: val->intval = POWER_SUPPLY_HEALTH_COOL; break; case BQ2562X_TEMP_COLD: val->intval = POWER_SUPPLY_HEALTH_COLD; break; case BQ2562X_TEMP_PIN_BIAS_REFER_FAULT: val->intval = POWER_SUPPLY_HEALTH_DEAD; break; } break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT: ret = bq2562x_get_ichg_curr(bq); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE: ret = bq2562x_get_chrg_volt(bq); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_PRECHARGE_CURRENT: ret = bq2562x_get_prechrg_curr(bq); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_CHARGE_TERM_CURRENT: ret = bq2562x_get_term_curr(bq); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_VOLTAGE_NOW: val->intval = state.vbus_adc; break; case POWER_SUPPLY_PROP_CURRENT_NOW: val->intval = state.ibus_adc; break; case POWER_SUPPLY_PROP_INPUT_VOLTAGE_LIMIT: ret = bq2562x_get_input_volt_lim(bq); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT: ret = bq2562x_get_input_curr_lim(bq); if (ret < 0) return ret; val->intval = ret; break; default: return -EINVAL; } return ret; } static int bq2562x_battery_get_property(struct power_supply *psy, enum power_supply_property psp, union power_supply_propval *val) { struct bq2562x_device *bq = power_supply_get_drvdata(psy); struct bq2562x_state state; int ret = 0; ret = bq2562x_get_state(bq, &state); if (ret) return ret; switch (psp) { case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT_MAX: val->intval = bq->init_data.ichg_max; break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE_MAX: val->intval = bq->init_data.vreg_max; break; case POWER_SUPPLY_PROP_VOLTAGE_NOW: val->intval = state.vbat_adc; break; case POWER_SUPPLY_PROP_CURRENT_NOW: val->intval = state.ibat_adc; break; default: return -EINVAL; } return ret; } static bool bq2562x_state_changed(struct bq2562x_device *bq, struct bq2562x_state *new_state) { struct bq2562x_state old_state; mutex_lock(&bq->lock); old_state = bq->state; mutex_unlock(&bq->lock); return memcmp(&old_state, new_state, sizeof(struct bq2562x_state)) != 0; } static irqreturn_t bq2562x_irq_handler_thread(int irq, void *private) { struct bq2562x_device *bq = private; struct bq2562x_state state; int ret; ret = bq2562x_get_state(bq, &state); if (ret < 0) goto irq_out; if (!bq2562x_state_changed(bq, &state)) goto irq_out; mutex_lock(&bq->lock); bq->state = state; mutex_unlock(&bq->lock); power_supply_changed(bq->charger); irq_out: return IRQ_HANDLED; } static enum power_supply_property bq2562x_power_supply_props[] = { POWER_SUPPLY_PROP_MANUFACTURER, POWER_SUPPLY_PROP_MODEL_NAME, POWER_SUPPLY_PROP_STATUS, POWER_SUPPLY_PROP_ONLINE, POWER_SUPPLY_PROP_HEALTH, POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT, POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE, POWER_SUPPLY_PROP_PRECHARGE_CURRENT, POWER_SUPPLY_PROP_CHARGE_TERM_CURRENT, POWER_SUPPLY_PROP_VOLTAGE_NOW, POWER_SUPPLY_PROP_INPUT_VOLTAGE_LIMIT, POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT, POWER_SUPPLY_PROP_CHARGE_TYPE, POWER_SUPPLY_PROP_USB_TYPE, POWER_SUPPLY_PROP_CURRENT_NOW, }; static enum power_supply_property bq2562x_battery_props[] = { POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT_MAX, POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE_MAX, POWER_SUPPLY_PROP_VOLTAGE_NOW, POWER_SUPPLY_PROP_CURRENT_NOW, }; static int bq2562x_property_is_writeable(struct power_supply *psy, enum power_supply_property prop) { switch (prop) { case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT: case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE: case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT: case POWER_SUPPLY_PROP_PRECHARGE_CURRENT: case POWER_SUPPLY_PROP_CHARGE_TERM_CURRENT: case POWER_SUPPLY_PROP_INPUT_VOLTAGE_LIMIT: return true; default: return false; } } static const struct power_supply_desc bq2562x_power_supply_desc = { .name = "bq2562x-charger", .type = POWER_SUPPLY_TYPE_USB, .usb_types = bq2562x_usb_type, .num_usb_types = ARRAY_SIZE(bq2562x_usb_type), .properties = bq2562x_power_supply_props, .num_properties = ARRAY_SIZE(bq2562x_power_supply_props), .get_property = bq2562x_get_property, .set_property = bq2562x_set_property, .property_is_writeable = bq2562x_property_is_writeable, }; static const struct power_supply_desc bq2562x_battery_desc = { .name = "bq2562x-battery", .type = POWER_SUPPLY_TYPE_BATTERY, .get_property = bq2562x_battery_get_property, .properties = bq2562x_battery_props, .num_properties = ARRAY_SIZE(bq2562x_battery_props), }; static bool bq2562x_is_volatile_reg(struct device *dev, unsigned int reg) { switch (reg) { case BQ2562X_CHRG_STAT_0...BQ2562X_FAULT_FLAG_0: case BQ2562X_ADC_IBUS_MSB...BQ2562X_ADC_TDIE_LSB: case BQ2562X_CHRG_CTRL_0: return true; default: return false; } } static const struct regmap_config bq25620_regmap_config = { .reg_bits = 8, .val_bits = 8, .max_register = BQ2562X_PART_INFO, .reg_defaults = bq25620_reg_defs, .num_reg_defaults = ARRAY_SIZE(bq25620_reg_defs), .cache_type = REGCACHE_FLAT, .volatile_reg = bq2562x_is_volatile_reg, }; static const struct regmap_config bq25622_regmap_config = { .reg_bits = 8, .val_bits = 8, .max_register = BQ2562X_PART_INFO, .reg_defaults = bq25622_reg_defs, .num_reg_defaults = ARRAY_SIZE(bq25622_reg_defs), .cache_type = REGCACHE_FLAT, .volatile_reg = bq2562x_is_volatile_reg, }; static int bq2562x_power_supply_init(struct bq2562x_device *bq, struct power_supply_config *psy_cfg, struct device *dev) { bq->charger = devm_power_supply_register(bq->dev, &bq2562x_power_supply_desc, psy_cfg); if (IS_ERR(bq->charger)) return -EINVAL; bq->battery = devm_power_supply_register(bq->dev, &bq2562x_battery_desc, psy_cfg); if (IS_ERR(bq->battery)) return -EINVAL; return 0; } static int bq2562x_hw_init(struct bq2562x_device *bq) { //struct power_supply_battery_info bat_info = { }; //TESSOLVE struct power_supply_battery_info *bat_info; int wd_reg_val = BQ2562X_WATCHDOG_DIS; int wd_max_val = BQ2562X_NUM_WD_VAL - 1; int ret = 0; int i; if (bq->watchdog_timer) { if (bq->watchdog_timer >= bq2562x_watchdog_time[wd_max_val]) wd_reg_val = wd_max_val; else { for (i = 0; i < wd_max_val; i++) { if (bq->watchdog_timer > bq2562x_watchdog_time[i] && bq->watchdog_timer < bq2562x_watchdog_time[i + 1]) { wd_reg_val = i; break; } } } } ret = regmap_update_bits(bq->regmap, BQ2562X_CHRG_CTRL_0, BQ2562X_WATCHDOG_MASK, wd_reg_val); if (ret) return ret; ret = power_supply_get_battery_info(bq->charger, &bat_info); if (ret) { dev_warn(bq->dev, "battery info missing, default values will be applied\n"); bat_info->constant_charge_current_max_ua = BQ2562X_ICHRG_I_DEF_uA; bat_info->constant_charge_voltage_max_uv = BQ2562X_VREG_V_DEF_uV; bat_info->precharge_current_ua = BQ2562X_PRECHRG_I_DEF_uA; bat_info->charge_term_current_ua = BQ2562X_TERMCHRG_I_DEF_uA; bq->init_data.ichg_max = BQ2562X_ICHRG_I_MAX_uA; bq->init_data.vreg_max = BQ2562X_VREG_V_MAX_uV; } else { bq->init_data.ichg_max = bat_info->constant_charge_current_max_ua; bq->init_data.vreg_max = bat_info->constant_charge_voltage_max_uv; } ret = bq2562x_set_ichrg_curr(bq, bat_info->constant_charge_current_max_ua); if (ret) return ret; ret = bq2562x_set_prechrg_curr(bq, bat_info->precharge_current_ua); if (ret) return ret; ret = bq2562x_set_chrg_volt(bq, bat_info->constant_charge_voltage_max_uv); if (ret) return ret; ret = bq2562x_set_term_curr(bq, bat_info->charge_term_current_ua); if (ret) return ret; ret = bq2562x_set_input_volt_lim(bq, bq->init_data.vlim); if (ret) return ret; ret = bq2562x_set_input_curr_lim(bq, bq->init_data.ilim); if (ret) return ret; power_supply_put_battery_info(bq->charger, bat_info); // TESSOLVE START ret = regmap_write(bq->regmap, BQ2562X_CHRG_CTRL_0, 0xa1); //0x16 register if (ret) return ret; ret = regmap_write(bq->regmap, BQ2562X_CHRG_CTRL_3, 0xc8); //0x19 register if (ret) return ret; //ret = regmap_write(bq->regmap, BQ2562X_NTC_CTRL_0, 0xbf); //0x1a register //if (ret) // return ret; ret = regmap_write(bq->regmap, BQ2562X_ADC_CTRL, 0xB0); //0x26 register if (ret) return ret; //TESSOLVE END return 0; } static int bq2562x_parse_dt(struct bq2562x_device *bq, struct power_supply_config *psy_cfg, struct device *dev) { int ret = 0; psy_cfg->drv_data = bq; psy_cfg->of_node = dev->of_node; ret = device_property_read_u32(bq->dev, "ti,watchdog-timeout-ms", &bq->watchdog_timer); if (ret) bq->watchdog_timer = BQ2562X_WATCHDOG_DIS; if (bq->watchdog_timer > BQ2562X_WATCHDOG_MAX || bq->watchdog_timer < BQ2562X_WATCHDOG_DIS) return -EINVAL; ret = device_property_read_u32(bq->dev, "input-voltage-limit-microvolt", &bq->init_data.vlim); if (ret) bq->init_data.vlim = BQ2562X_VINDPM_DEF_uV; if (bq->init_data.vlim > BQ2562X_VINDPM_V_MAX_uV || bq->init_data.vlim < BQ2562X_VINDPM_V_MIN_uV) return -EINVAL; ret = device_property_read_u32(bq->dev, "input-current-limit-microamp", &bq->init_data.ilim); if (ret) bq->init_data.ilim = BQ2562X_IINDPM_DEF_uA; if (bq->init_data.ilim > BQ2562X_IINDPM_I_MAX_uA || bq->init_data.ilim < BQ2562X_IINDPM_I_MIN_uA) return -EINVAL; bq->ac_detect_gpio = devm_gpiod_get_optional(bq->dev, "ac-detect", GPIOD_IN); if (IS_ERR(bq->ac_detect_gpio)) { ret = PTR_ERR(bq->ac_detect_gpio); dev_err(bq->dev, "Failed to get ac detect"); //return ret; return 0; //TESSOLVE } bq->ce_gpio = devm_gpiod_get_optional(bq->dev, "charge-enable", GPIOD_OUT_LOW); if (IS_ERR(bq->ce_gpio)) { ret = PTR_ERR(bq->ce_gpio); dev_err(bq->dev, "Failed to get ce"); //return ret; return 0; //TESSOLVE } return 0; } static int bq2562x_probe(struct i2c_client *client, const struct i2c_device_id *id) { struct device *dev = &client->dev; struct bq2562x_device *bq; struct power_supply_config psy_cfg = { }; int ret; #ifdef CONFIG_INTERRUPT_AS_GPIO int irq_gpio, irqn; #endif bq = devm_kzalloc(dev, sizeof(*bq), GFP_KERNEL); if (!bq) return -ENOMEM; bq->client = client; bq->dev = dev; mutex_init(&bq->lock); strncpy(bq->model_name, id->name, I2C_NAME_SIZE); bq->device_id = id->driver_data; switch (bq->device_id) { case BQ25620: bq->regmap = devm_regmap_init_i2c(client, &bq25620_regmap_config); break; case BQ25622: bq->regmap = devm_regmap_init_i2c(client, &bq25620_regmap_config); break; } if (IS_ERR(bq->regmap)) { dev_err(dev, "Failed to allocate register map\n"); return PTR_ERR(bq->regmap); } i2c_set_clientdata(client, bq); //TESSOLVE; start gpio_num = of_get_gpio(client->dev.of_node, 0); if (gpio_num < 0) { printk("Failed to parse GPIO number\n"); return gpio_num; } printk("GPIO number for Battery CE pin %d \n",gpio_num); // Request the GPIO pin ret = gpio_request(gpio_num, "CE-GPIO"); if (ret) { printk("Failed to request GPIO: %d\n", ret); return ret; } ret = gpio_direction_output(gpio_num, 0); if (ret) { printk("Failed to set GPIO direction/output: %d\n", ret); gpio_free(gpio_num); return ret; } //TESSOLVE END ret = bq2562x_parse_dt(bq, &psy_cfg, dev); if (ret) { dev_err(dev, "Failed to read device tree properties%d\n", ret); return ret; } ret = devm_add_action_or_reset(dev, bq2562x_charger_reset, bq); if (ret) return ret; /* OTG reporting */ bq->usb2_phy = devm_usb_get_phy(dev, USB_PHY_TYPE_USB2); if (!IS_ERR_OR_NULL(bq->usb2_phy)) { INIT_WORK(&bq->usb_work, bq2562x_usb_work); bq->usb_nb.notifier_call = bq2562x_usb_notifier; usb_register_notifier(bq->usb2_phy, &bq->usb_nb); } bq->usb3_phy = devm_usb_get_phy(dev, USB_PHY_TYPE_USB3); if (!IS_ERR_OR_NULL(bq->usb3_phy)) { INIT_WORK(&bq->usb_work, bq2562x_usb_work); bq->usb_nb.notifier_call = bq2562x_usb_notifier; usb_register_notifier(bq->usb3_phy, &bq->usb_nb); } #ifdef CONFIG_INTERRUPT_AS_GPIO irq_gpio = of_get_named_gpio(client->dev.of_node, "ti,irq-gpio", 0); if (!gpio_is_valid(irq_gpio)) { dev_err(bq->dev, "%s: %d gpio get failed\n", __func__, irq_gpio); return -EINVAL; } ret = gpio_request(irq_gpio, "bq2562x irq pin"); if (ret) { dev_err(bq->dev, "%s: %d gpio request failed\n", __func__, irq_gpio); return ret; } gpio_direction_input(irq_gpio); irqn = gpio_to_irq(irq_gpio); if (irqn < 0) { dev_err(bq->dev, "%s:%d gpio_to_irq failed\n", __func__, irqn); return irqn; } client->irq = irqn; #endif if (client->irq) { ret = devm_request_threaded_irq(dev, client->irq, NULL, bq2562x_irq_handler_thread, IRQF_TRIGGER_FALLING | IRQF_ONESHOT, dev_name(&client->dev), bq); if (ret < 0) { dev_err(dev, "get irq fail: %d\n", ret); return ret; } } ret = bq2562x_power_supply_init(bq, &psy_cfg, dev); if (ret) { dev_err(dev, "Failed to register power supply\n"); return ret; } ret = bq2562x_hw_init(bq); if (ret) { dev_err(dev, "Cannot initialize the chip.\n"); return ret; } return ret; } static const struct i2c_device_id bq2562x_i2c_ids[] = { { "bq25620", BQ25620 }, { "bq25622", BQ25622 }, {}, }; MODULE_DEVICE_TABLE(i2c, bq2562x_i2c_ids); static const struct of_device_id bq2562x_of_match[] = { { .compatible = "ti,bq25620", }, { .compatible = "ti,bq25622", }, { }, }; MODULE_DEVICE_TABLE(of, bq2562x_of_match); static const struct acpi_device_id bq2562x_acpi_match[] = { { "bq25620", BQ25620 }, { "bq25622", BQ25622 }, {}, }; MODULE_DEVICE_TABLE(acpi, bq2562x_acpi_match); static struct i2c_driver bq2562x_driver = { .driver = { .name = "bq2562x-charger", .of_match_table = bq2562x_of_match, .acpi_match_table = bq2562x_acpi_match, }, .probe = bq2562x_probe, .id_table = bq2562x_i2c_ids, }; module_i2c_driver(bq2562x_driver); MODULE_AUTHOR("Texas Instruments"); MODULE_DESCRIPTION("bq2562x charger driver"); MODULE_LICENSE("GPL v2");
DTS changes are below
bat: battery {
compatible = "simple-battery";
constant-charge-current-max-microamp = <1040000>;
constant-charge-voltage-max-microvolt = <4200000>;
precharge-current-microamp = <100000>;
charge-term-current-microamp = <60000>;
};
bq25622: charger@6b {
compatible = "ti,bq25622";
reg = <0x6b>;
pinctrl-names = "default";
pinctrl-0 = <&main_charger_pins>;
interrupt-parent = <&main_gpio0>;
gpios = <&main_gpio0 50 GPIO_ACTIVE_LOW>;
interrupts =<49 IRQ_TYPE_EDGE_FALLING>;
ti,watchdog-timeout-ms = <40000>;
input-current-limit-microamp = <1000000>;
input-voltage-limit-microvolt = <4600000>;
monitored-battery = <&bat>;
//interrupt-cells = <2>;
//ac-detect-gpios = <&main_gpio0 50 GPIO_ACTIVE_LOW>;
//charge-enable-gpios = <&main_gpio0 50 GPIO_ACTIVE_LOW>;
//ti,watchdog-timeout-ms = <40000>;
//input-current-limit-microamp = <1000000>;
//input-voltage-limit-microvolt = <4600000>;
};
Thanks,
Naresh
HI Ning ,
Thanks for attatching driver .
I am attaching my changes in the driver , which makes me charging , discarging and charging full showing bu i observed below issue.
letsay ,when i read the statuus charging , and battery current showing 2mA , after 10 min also showing same . if i reboot /power cycle only chagnes are reflecting ,
Kindly help me on this . its urgent.
my changes are done with name comment name "TESSOLVE" in driver .
// SPDX-License-Identifier: GPL-2.0 // BQ2562X driver // Copyright (C) 2020 Texas Instruments Incorporated - http://www.ti.com/ #include <linux/module.h> #include <linux/i2c.h> #include <linux/power_supply.h> #include <linux/regmap.h> #include <linux/types.h> #include <linux/gpio/consumer.h> #include <linux/interrupt.h> #include <linux/delay.h> #include <linux/usb/phy.h> #include <linux/acpi.h> #include <linux/of.h> #include <linux/gpio.h> #include <linux/of_gpio.h> #include "bq2562x_charger.h" #define BQ2562X_NUM_WD_VAL 4 int gpio_num; struct bq2562x_init_data { u32 ichg; u32 ilim; u32 vreg; u32 iterm; u32 iprechg; u32 vlim; u32 ichg_max; u32 vreg_max; }; struct bq2562x_state { bool online; u8 chrg_status; u8 chrg_type; u8 health; u8 chrg_fault; u8 vsys_status; u8 vbus_status; u8 fault_0; u8 fault_1; u32 vbat_adc; u32 vbus_adc; u32 ibat_adc; u32 ibus_adc; }; enum bq2562x_id { BQ25620, BQ25622, }; struct bq2562x_device { struct i2c_client *client; struct device *dev; struct power_supply *charger; struct power_supply *battery; struct mutex lock; struct usb_phy *usb2_phy; struct usb_phy *usb3_phy; struct notifier_block usb_nb; struct work_struct usb_work; unsigned long usb_event; struct regmap *regmap; char model_name[I2C_NAME_SIZE]; int device_id; struct gpio_desc *ac_detect_gpio; struct gpio_desc *ce_gpio; struct bq2562x_init_data init_data; struct bq2562x_state state; int watchdog_timer; }; static struct reg_default bq25620_reg_defs[] = { {BQ2562X_CHRG_I_LIM_MSB, 0x03}, {BQ2562X_CHRG_I_LIM_LSB, 0x40}, {BQ2562X_CHRG_V_LIM_MSB, 0x0D}, {BQ2562X_CHRG_V_LIM_LSB, 0x20}, {BQ2562X_INPUT_I_LIM_MSB, 0x0A}, {BQ2562X_INPUT_I_LIM_LSB, 0x00}, {BQ2562X_INPUT_V_LIM_MSB, 0x0E}, {BQ2562X_INPUT_V_LIM_LSB, 0x60}, {BQ2562X_IOTG_MSB, 0x03}, {BQ2562X_IOTG_LSB, 0x20}, {BQ2562X_VOTG_MSB, 0x0F}, {BQ2562X_VOTG_LSB, 0xC0}, {BQ2562X_MIN_SYS_V_MSB, 0x0B}, {BQ2562X_MIN_SYS_V_LSB, 0x00}, {BQ2562X_PRECHRG_CTRL_MSB, 0x00}, {BQ2562X_PRECHRG_CTRL_LSB, 0x50}, {BQ2562X_TERM_CTRL_MSB, 0x00}, {BQ2562X_TERM_CTRL_LSB, 0x30}, {BQ2562X_CHRG_CTRL, 0x06}, {BQ2562X_TIMER_CTRL, 0x5C}, {BQ2562X_CHRG_CTRL_0, 0xA1}, {BQ2562X_CHRG_CTRL_1, 0x4E}, {BQ2562X_CHRG_CTRL_2, 0x04}, {BQ2562X_CHRG_CTRL_3, 0xC4}, {BQ2562X_NTC_CTRL_0, 0x3D}, {BQ2562X_NTC_CTRL_1, 0x25}, {BQ2562X_NTC_CTRL_2, 0x3F}, {BQ2562X_CHRG_STAT_0, 0x00}, {BQ2562X_CHRG_STAT_1, 0x00}, {BQ2562X_FAULT_STAT_0, 0x00}, {BQ2562X_CHRG_FLAG_0, 0x00}, {BQ2562X_CHRG_FLAG_1, 0x00}, {BQ2562X_FAULT_FLAG_0, 0x00}, {BQ2562X_CHRG_MSK_0, 0x00}, {BQ2562X_CHRG_MSK_1, 0x00}, {BQ2562X_FAULT_MSK_0, 0x00}, {BQ2562X_ADC_CTRL, 0x30}, {BQ2562X_FN_DISABE_0, 0x00}, {BQ2562X_ADC_IBUS_MSB, 0x00}, {BQ2562X_ADC_IBUS_LSB, 0x00}, {BQ2562X_ADC_IBAT_MSB, 0x00}, {BQ2562X_ADC_IBAT_LSB, 0x00}, {BQ2562X_ADC_VBUS_MSB, 0x00}, {BQ2562X_ADC_VBUS_LSB, 0x00}, {BQ2562X_ADC_VPMID_MSB, 0x00}, {BQ2562X_ADC_VPMID_LSB, 0x00}, {BQ2562X_ADC_VBAT_MSB, 0x00}, {BQ2562X_ADC_VBAT_LSB, 0x00}, {BQ2562X_ADC_VSYS_MSB, 0x00}, {BQ2562X_ADC_VSYS_LSB, 0x00}, {BQ2562X_ADC_TS_MSB, 0x00}, {BQ2562X_ADC_TS_LSB, 0x00}, {BQ2562X_ADC_TDIE_MSB, 0x00}, {BQ2562X_ADC_TDIE_LSB, 0x00}, {BQ2562X_PART_INFO, 0x00}, }; static struct reg_default bq25622_reg_defs[] = { {BQ2562X_CHRG_I_LIM_MSB, 0x03}, {BQ2562X_CHRG_I_LIM_LSB, 0x40}, {BQ2562X_CHRG_V_LIM_MSB, 0x0D}, {BQ2562X_CHRG_V_LIM_LSB, 0x20}, {BQ2562X_INPUT_I_LIM_MSB, 0x0A}, {BQ2562X_INPUT_I_LIM_LSB, 0x00}, {BQ2562X_INPUT_V_LIM_MSB, 0x0E}, {BQ2562X_INPUT_V_LIM_LSB, 0x60}, {BQ2562X_IOTG_MSB, 0x03}, {BQ2562X_IOTG_LSB, 0x20}, {BQ2562X_VOTG_MSB, 0x0F}, {BQ2562X_VOTG_LSB, 0xC0}, {BQ2562X_MIN_SYS_V_MSB, 0x0B}, {BQ2562X_MIN_SYS_V_LSB, 0x00}, {BQ2562X_PRECHRG_CTRL_MSB, 0x00}, {BQ2562X_PRECHRG_CTRL_LSB, 0x50}, {BQ2562X_TERM_CTRL_MSB, 0x00}, {BQ2562X_TERM_CTRL_LSB, 0x30}, {BQ2562X_CHRG_CTRL, 0x06}, {BQ2562X_TIMER_CTRL, 0x5C}, {BQ2562X_CHRG_CTRL_0, 0xA1}, {BQ2562X_CHRG_CTRL_1, 0x4E}, {BQ2562X_CHRG_CTRL_2, 0x04}, {BQ2562X_CHRG_CTRL_3, 0xC4}, {BQ2562X_NTC_CTRL_0, 0x3D}, {BQ2562X_NTC_CTRL_1, 0x25}, {BQ2562X_NTC_CTRL_2, 0x3F}, {BQ2562X_CHRG_STAT_0, 0x00}, {BQ2562X_CHRG_STAT_1, 0x00}, {BQ2562X_FAULT_STAT_0, 0x00}, {BQ2562X_CHRG_FLAG_0, 0x00}, {BQ2562X_CHRG_FLAG_1, 0x00}, {BQ2562X_FAULT_FLAG_0, 0x00}, {BQ2562X_CHRG_MSK_0, 0x00}, {BQ2562X_CHRG_MSK_1, 0x00}, {BQ2562X_FAULT_MSK_0, 0x00}, {BQ2562X_ADC_CTRL, 0x30}, {BQ2562X_FN_DISABE_0, 0x00}, {BQ2562X_ADC_IBUS_MSB, 0x00}, {BQ2562X_ADC_IBUS_LSB, 0x00}, {BQ2562X_ADC_IBAT_MSB, 0x00}, {BQ2562X_ADC_IBAT_LSB, 0x00}, {BQ2562X_ADC_VBUS_MSB, 0x00}, {BQ2562X_ADC_VBUS_LSB, 0x00}, {BQ2562X_ADC_VPMID_MSB, 0x00}, {BQ2562X_ADC_VPMID_LSB, 0x00}, {BQ2562X_ADC_VBAT_MSB, 0x00}, {BQ2562X_ADC_VBAT_LSB, 0x00}, {BQ2562X_ADC_VSYS_MSB, 0x00}, {BQ2562X_ADC_VSYS_LSB, 0x00}, {BQ2562X_ADC_TS_MSB, 0x00}, {BQ2562X_ADC_TS_LSB, 0x00}, {BQ2562X_ADC_TDIE_MSB, 0x00}, {BQ2562X_ADC_TDIE_LSB, 0x00}, {BQ2562X_PART_INFO, 0x00}, }; static int bq2562x_watchdog_time[BQ2562X_NUM_WD_VAL] = {0, 40000, 80000, 160000}; static enum power_supply_usb_type bq2562x_usb_type[] = { POWER_SUPPLY_USB_TYPE_ACA, POWER_SUPPLY_USB_TYPE_SDP, POWER_SUPPLY_USB_TYPE_CDP, POWER_SUPPLY_USB_TYPE_DCP, POWER_SUPPLY_USB_TYPE_UNKNOWN, }; static int bq2562x_usb_notifier(struct notifier_block *nb, unsigned long val, void *priv) { struct bq2562x_device *bq = container_of(nb, struct bq2562x_device, usb_nb); bq->usb_event = val; queue_work(system_power_efficient_wq, &bq->usb_work); return NOTIFY_OK; } static void bq2562x_usb_work(struct work_struct *data) { struct bq2562x_device *bq = container_of(data, struct bq2562x_device, usb_work); switch (bq->usb_event) { case USB_EVENT_ID: break; case USB_EVENT_NONE: power_supply_changed(bq->charger); break; } } static bool bq2562x_get_charge_enable(struct bq2562x_device *bq) { int ret; int ce_pin; int charger_enable; int chrg_ctrl_0; if (bq->ce_gpio) ce_pin = gpiod_get_value_cansleep(bq->ce_gpio); ret = gpio_direction_output(gpio_num, 0); //TESSOLVE ret = regmap_read(bq->regmap, BQ2562X_CHRG_CTRL_0, &chrg_ctrl_0); if (ret) return ret; charger_enable = chrg_ctrl_0 & BQ2562X_CHRG_EN; if (charger_enable) { if (bq->ce_gpio && !ce_pin) return true; } //return false; return true; //TESSOLVE } static int bq2562x_set_charge_enable(struct bq2562x_device *bq, int val) { gpiod_set_value_cansleep(bq->ce_gpio, !val); //gpio_direction_output(gpio_num, !val); //TESSOLVE return regmap_update_bits(bq->regmap, BQ2562X_CHRG_CTRL_0, BQ2562X_CHRG_EN, val); } static int bq2562x_get_vbat_adc(struct bq2562x_device *bq) { int ret; int vbat_adc_lsb, vbat_adc_msb; u16 vbat_adc; ret = regmap_read(bq->regmap, BQ2562X_ADC_VBAT_LSB, &vbat_adc_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_ADC_VBAT_MSB, &vbat_adc_msb); if (ret) return ret; vbat_adc = ((vbat_adc_msb << 8) | vbat_adc_lsb) >> BQ2562X_ADC_VBAT_MOVE_STEP; return vbat_adc * BQ2562X_ADC_VBAT_STEP_uV; } static int bq2562x_get_vbus_adc(struct bq2562x_device *bq) { int ret; int vbus_adc_lsb, vbus_adc_msb; u16 vbus_adc; ret = regmap_read(bq->regmap, BQ2562X_ADC_VBUS_LSB, &vbus_adc_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_ADC_VBUS_MSB, &vbus_adc_msb); if (ret) return ret; vbus_adc = ((vbus_adc_msb << 8) | vbus_adc_lsb) >> BQ2562X_ADC_VBUS_MOVE_STEP; return vbus_adc * BQ2562X_ADC_VBUS_STEP_uV; } static int bq2562x_get_ibat_adc(struct bq2562x_device *bq) { int ret; int ibat_adc_lsb, ibat_adc_msb; u16 ibat_adc; ret = regmap_read(bq->regmap, BQ2562X_ADC_IBAT_LSB, &ibat_adc_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_ADC_IBAT_MSB, &ibat_adc_msb); if (ret) return ret; ibat_adc = ((ibat_adc_msb << 8) | ibat_adc_lsb) >> BQ2562X_ADC_IBAT_MOVE_STEP; return ibat_adc * BQ2562X_ADC_IBAT_STEP_uV; } static int bq2562x_get_ibus_adc(struct bq2562x_device *bq) { int ret; int ibus_adc_lsb, ibus_adc_msb; int ibus_adc; ret = regmap_read(bq->regmap, BQ2562X_ADC_IBUS_LSB, &ibus_adc_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_ADC_IBUS_MSB, &ibus_adc_msb); if (ret) return ret; ibus_adc = ((ibus_adc_msb << 8) | ibus_adc_lsb) >> BQ2562X_ADC_IBUS_MOVE_STEP; return ibus_adc * BQ2562X_ADC_CURR_STEP_uA; } static int bq2562x_get_term_curr(struct bq2562x_device *bq) { int ret; int iterm_lsb, iterm_msb; u16 iterm; ret = regmap_read(bq->regmap, BQ2562X_TERM_CTRL_LSB, &iterm_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_TERM_CTRL_MSB, &iterm_msb); if (ret) return ret; iterm = ((iterm_msb << 8) | iterm_lsb) >> BQ2562X_ITERM_MOVE_STEP; return iterm * BQ2562X_TERMCHRG_CURRENT_STEP_uA; } static int bq2562x_get_prechrg_curr(struct bq2562x_device *bq) { int ret; int prechrg_curr_lsb, prechrg_curr_msb; u16 prechrg_curr; ret = regmap_read(bq->regmap, BQ2562X_PRECHRG_CTRL_LSB, &prechrg_curr_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_PRECHRG_CTRL_MSB, &prechrg_curr_msb); if (ret) return ret; prechrg_curr = ((prechrg_curr_msb << 8) | prechrg_curr_lsb) >> BQ2562X_PRECHRG_MOVE_STEP; return prechrg_curr * BQ2562X_PRECHRG_CURRENT_STEP_uA; } static int bq2562x_get_ichg_curr(struct bq2562x_device *bq) { int ret; int ichg, ichg_lsb, ichg_msb; ret = regmap_read(bq->regmap, BQ2562X_CHRG_I_LIM_MSB, &ichg_msb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_CHRG_I_LIM_LSB, &ichg_lsb); if (ret) return ret; ichg = ((ichg_msb << 8) | ichg_lsb) >> BQ2562X_ICHG_MOVE_STEP; return ichg * BQ2562X_ICHRG_CURRENT_STEP_uA; } static int bq2562x_set_term_curr(struct bq2562x_device *bq, int term_current) { int reg_val; int term_curr_msb, term_curr_lsb; int ret; term_current = clamp(term_current, BQ2562X_TERMCHRG_I_MIN_uA, BQ2562X_TERMCHRG_I_MAX_uA); reg_val = (term_current / BQ2562X_TERMCHRG_CURRENT_STEP_uA) << BQ2562X_ITERM_MOVE_STEP; term_curr_msb = (reg_val >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_TERM_CTRL_MSB, term_curr_msb); if (ret) return ret; term_curr_lsb = reg_val & 0xff; return regmap_write(bq->regmap, BQ2562X_TERM_CTRL_LSB, term_curr_lsb); } static int bq2562x_set_prechrg_curr(struct bq2562x_device *bq, int pre_current) { int reg_val; int prechrg_curr_msb, prechrg_curr_lsb; int ret; pre_current = clamp(pre_current, BQ2562X_PRECHRG_I_MIN_uA, BQ2562X_PRECHRG_I_MAX_uA); bq2562x_set_charge_enable(bq, 0); reg_val = (pre_current / BQ2562X_PRECHRG_CURRENT_STEP_uA) << BQ2562X_PRECHRG_MOVE_STEP; prechrg_curr_msb = (reg_val >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_PRECHRG_CTRL_MSB, prechrg_curr_msb); if (ret) return ret; prechrg_curr_lsb = reg_val & 0xff; ret = regmap_write(bq->regmap, BQ2562X_PRECHRG_CTRL_LSB, prechrg_curr_lsb); if (ret) return ret; return bq2562x_set_charge_enable(bq, 1); } static int bq2562x_set_ichrg_curr(struct bq2562x_device *bq, int chrg_curr) { int chrg_curr_max = bq->init_data.ichg_max; int ichg, ichg_msb, ichg_lsb; int ret; chrg_curr = clamp(chrg_curr, BQ2562X_ICHRG_I_MIN_uA, chrg_curr_max); bq2562x_set_charge_enable(bq, 0); ichg = ((chrg_curr / BQ2562X_ICHRG_CURRENT_STEP_uA) << BQ2562X_ICHG_MOVE_STEP); ichg_msb = (ichg >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_CHRG_I_LIM_MSB, ichg_msb); if (ret) return ret; ichg_lsb = ichg & 0xff; ret = regmap_write(bq->regmap, BQ2562X_CHRG_I_LIM_LSB, ichg_lsb); if (ret) return ret; return bq2562x_set_charge_enable(bq, 1); } static int bq2562x_set_chrg_volt(struct bq2562x_device *bq, int chrg_volt) { int chrg_volt_max = bq->init_data.vreg_max; int chrg_volt_lsb, chrg_volt_msb, vlim; int ret; chrg_volt = clamp(chrg_volt, BQ2562X_VREG_V_MIN_uV, chrg_volt_max); vlim = (chrg_volt / BQ2562X_VREG_V_STEP_uV) << BQ2562X_CHRG_V_LIM_MOVE_STEP; chrg_volt_msb = (vlim >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_CHRG_V_LIM_MSB, chrg_volt_msb); if (ret) return ret; chrg_volt_lsb = vlim & 0xff; return regmap_write(bq->regmap, BQ2562X_CHRG_V_LIM_LSB, chrg_volt_lsb); } static int bq2562x_get_chrg_volt(struct bq2562x_device *bq) { int ret; int chrg_volt_lsb, chrg_volt_msb, chrg_volt; ret = regmap_read(bq->regmap, BQ2562X_CHRG_V_LIM_LSB, &chrg_volt_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_CHRG_V_LIM_MSB, &chrg_volt_msb); if (ret) return ret; chrg_volt = ((chrg_volt_msb << 8) | chrg_volt_lsb) >> BQ2562X_CHRG_V_LIM_MOVE_STEP; return chrg_volt * BQ2562X_VREG_V_STEP_uV; } static int bq2562x_set_input_volt_lim(struct bq2562x_device *bq, int vindpm) { int ret; int vlim_lsb, vlim_msb; int vlim; vindpm = clamp(vindpm, BQ2562X_VINDPM_V_MIN_uV, BQ2562X_VINDPM_V_MAX_uV); vlim = (vindpm / BQ2562X_VINDPM_STEP_uV) << BQ2562X_INPUT_V_LIM_MOVE_STEP; vlim_msb = (vlim >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_INPUT_V_LIM_MSB, vlim_msb); if (ret) return ret; vlim_lsb = vlim & 0xff; return regmap_write(bq->regmap, BQ2562X_INPUT_V_LIM_LSB, vlim_lsb); } static int bq2562x_get_input_volt_lim(struct bq2562x_device *bq) { int ret; int vlim; int vlim_lsb, vlim_msb; ret = regmap_read(bq->regmap, BQ2562X_INPUT_V_LIM_LSB, &vlim_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_INPUT_V_LIM_MSB, &vlim_msb); if (ret) return ret; vlim = ((vlim_msb << 8) | vlim_lsb) >> BQ2562X_INPUT_V_LIM_MOVE_STEP; return vlim * BQ2562X_VINDPM_STEP_uV; } static int bq2562x_set_input_curr_lim(struct bq2562x_device *bq, int iindpm) { int ret; int ilim, ilim_lsb, ilim_msb; iindpm = clamp(iindpm, BQ2562X_IINDPM_I_MIN_uA, BQ2562X_IINDPM_I_MAX_uA); ilim = (iindpm / BQ2562X_IINDPM_STEP_uA) << BQ2562X_INPUT_I_LIM__MOVE_STEP; ilim_lsb = ilim & 0xff; ret = regmap_write(bq->regmap, BQ2562X_INPUT_I_LIM_LSB, ilim_lsb); if (ret) return ret; ilim_msb = (ilim >> 8) & 0xff; ret = regmap_write(bq->regmap, BQ2562X_INPUT_I_LIM_MSB, ilim_msb); return ret; } static int bq2562x_get_input_curr_lim(struct bq2562x_device *bq) { int ret; int ilim_msb, ilim_lsb; u16 ilim; ret = regmap_read(bq->regmap, BQ2562X_INPUT_I_LIM_LSB, &ilim_lsb); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_INPUT_I_LIM_MSB, &ilim_msb); if (ret) return ret; ilim = ((ilim_msb << 8) | ilim_lsb) >> BQ2562X_INPUT_I_LIM__MOVE_STEP; return ilim * BQ2562X_IINDPM_STEP_uA; } static int bq2562x_get_online_status(struct bq2562x_device *bq) { int ret; int chrg_stat_1; int online_status; ret = regmap_update_bits(bq->regmap, BQ2562X_CHRG_STAT_1, BQ2562X_VBUS_STAT_MSK, BQ2562X_UNKNOWN_500MA); if (ret) return ret; ret = regmap_read(bq->regmap, BQ2562X_CHRG_STAT_1, &chrg_stat_1); if (ret) return ret; online_status = chrg_stat_1 & BQ2562X_VBUS_STAT_MSK; if ((online_status == BQ2562X_USB_SDP) || (online_status == BQ2562X_OTG_MODE)) online_status = 0; else online_status = 1; return online_status; } static int bq2562x_get_state(struct bq2562x_device *bq, struct bq2562x_state *state) { int chrg_stat_0, chrg_stat_1; int fault_0, fault_1; int ret; int val = 0; ret = regmap_update_bits(bq->regmap, BQ2562X_ADC_CTRL, BQ2562X_ADC_EN, BQ2562X_ADC_EN); if (ret) return ret; if (bq->ac_detect_gpio) { val = gpiod_get_value_cansleep(bq->ac_detect_gpio); state->vbus_status = val; } ret = regmap_read(bq->regmap, BQ2562X_CHRG_STAT_1, &chrg_stat_1); if (ret) return ret; if (bq2562x_get_charge_enable(bq)) state->chrg_status = chrg_stat_1 & BQ2562X_CHG_STAT_MSK; else state->chrg_status = BQ2562X_NOT_CHRGING; state->chrg_type = chrg_stat_1 & BQ2562X_VBUS_STAT_MSK; ret = regmap_read(bq->regmap, BQ2562X_FAULT_STAT_0, &fault_0); if (ret) return ret; state->health = fault_0 & BQ2562X_TEMP_MASK; state->fault_0 = fault_0; ret = regmap_read(bq->regmap, BQ2562X_FAULT_STAT_0, &fault_1); if (ret) return ret; state->fault_1 = fault_1; ret = regmap_read(bq->regmap, BQ2562X_CHRG_STAT_0, &chrg_stat_0); if (ret) return ret; state->online = bq2562x_get_online_status(bq); state->vbat_adc = bq2562x_get_vbat_adc(bq); state->vbus_adc = bq2562x_get_vbus_adc(bq); state->ibat_adc = bq2562x_get_ibat_adc(bq); state->ibus_adc = bq2562x_get_ibus_adc(bq); return 0; } static void bq2562x_charger_reset(void *data) { struct bq2562x_device *bq = data; if (!IS_ERR_OR_NULL(bq->usb2_phy)) usb_unregister_notifier(bq->usb2_phy, &bq->usb_nb); if (!IS_ERR_OR_NULL(bq->usb3_phy)) usb_unregister_notifier(bq->usb3_phy, &bq->usb_nb); } static int bq2562x_set_property(struct power_supply *psy, enum power_supply_property prop, const union power_supply_propval *val) { struct bq2562x_device *bq = power_supply_get_drvdata(psy); int ret = -EINVAL; switch (prop) { case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT: ret = bq2562x_set_input_curr_lim(bq, val->intval); break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE: ret = bq2562x_set_chrg_volt(bq, val->intval); break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT: ret = bq2562x_set_ichrg_curr(bq, val->intval); break; case POWER_SUPPLY_PROP_PRECHARGE_CURRENT: ret = bq2562x_set_prechrg_curr(bq, val->intval); break; case POWER_SUPPLY_PROP_CHARGE_TERM_CURRENT: ret = bq2562x_set_term_curr(bq, val->intval); break; case POWER_SUPPLY_PROP_INPUT_VOLTAGE_LIMIT: ret = bq2562x_set_input_volt_lim(bq, val->intval); break; default: return -EINVAL; } return ret; } static int bq2562x_get_property(struct power_supply *psy, enum power_supply_property psp, union power_supply_propval *val) { struct bq2562x_device *bq = power_supply_get_drvdata(psy); struct bq2562x_state state; int ret = 0; ret = bq2562x_get_state(bq, &state); if (ret) return ret; switch (psp) { case POWER_SUPPLY_PROP_STATUS: if (!state.chrg_type || (state.chrg_type == BQ2562X_OTG_MODE)) val->intval = POWER_SUPPLY_STATUS_DISCHARGING; else if (!state.chrg_status) { val->intval = POWER_SUPPLY_STATUS_NOT_CHARGING; if (bq2562x_get_chrg_volt(bq) >= (state.vbat_adc - BQ2562X_ADC_VBAT_STEP_uV)) val->intval = POWER_SUPPLY_STATUS_FULL; } //else if (state.chrg_status == BQ2562X_TERM_CHRG) // val->intval = POWER_SUPPLY_STATUS_FULL; else val->intval = POWER_SUPPLY_STATUS_CHARGING; break; case POWER_SUPPLY_PROP_CHARGE_TYPE: switch (state.chrg_status) { case BQ2562X_TRICKLE_CHRG: val->intval = POWER_SUPPLY_CHARGE_TYPE_TRICKLE; break; case BQ2562X_TAPER_CHRG: val->intval = POWER_SUPPLY_CHARGE_TYPE_STANDARD; break; case BQ2562X_TOP_OFF_CHRG: val->intval = POWER_SUPPLY_CHARGE_TYPE_TRICKLE; break; case BQ2562X_NOT_CHRGING: val->intval = POWER_SUPPLY_CHARGE_TYPE_NONE; break; default: val->intval = POWER_SUPPLY_CHARGE_TYPE_UNKNOWN; } break; case POWER_SUPPLY_PROP_MANUFACTURER: val->strval = BQ2562X_MANUFACTURER; break; case POWER_SUPPLY_PROP_MODEL_NAME: val->strval = bq->model_name; break; case POWER_SUPPLY_PROP_ONLINE: val->intval = state.online; break; case POWER_SUPPLY_PROP_USB_TYPE: if (!state.chrg_type) { val->intval = POWER_SUPPLY_USB_TYPE_UNKNOWN; break; } switch (state.chrg_type) { case BQ2562X_USB_SDP: val->intval = POWER_SUPPLY_USB_TYPE_SDP; break; case BQ2562X_USB_CDP: val->intval = POWER_SUPPLY_USB_TYPE_CDP; break; case BQ2562X_USB_DCP: val->intval = POWER_SUPPLY_USB_TYPE_DCP; break; case BQ2562X_OTG_MODE: val->intval = POWER_SUPPLY_USB_TYPE_ACA; break; default: val->intval = POWER_SUPPLY_USB_TYPE_UNKNOWN; break; } break; case POWER_SUPPLY_PROP_HEALTH: if (state.fault_1 & (BQ2562X_OTG_FAULT_STAT | BQ2562X_SYS_FAULT_STAT)) val->intval = POWER_SUPPLY_HEALTH_OVERVOLTAGE; else val->intval = POWER_SUPPLY_HEALTH_GOOD; switch (state.health) { case BQ2562X_TEMP_TS_NORMAL: val->intval = POWER_SUPPLY_HEALTH_GOOD; break; case BQ2562X_TEMP_HOT: val->intval = POWER_SUPPLY_HEALTH_HOT; break; case BQ2562X_TEMP_WARM: case BQ2562X_TEMP_PREWARM: val->intval = POWER_SUPPLY_HEALTH_WARM; break; case BQ2562X_TEMP_COOL: case BQ2562X_TEMP_PRECOOL: val->intval = POWER_SUPPLY_HEALTH_COOL; break; case BQ2562X_TEMP_COLD: val->intval = POWER_SUPPLY_HEALTH_COLD; break; case BQ2562X_TEMP_PIN_BIAS_REFER_FAULT: val->intval = POWER_SUPPLY_HEALTH_DEAD; break; } break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT: ret = bq2562x_get_ichg_curr(bq); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE: ret = bq2562x_get_chrg_volt(bq); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_PRECHARGE_CURRENT: ret = bq2562x_get_prechrg_curr(bq); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_CHARGE_TERM_CURRENT: ret = bq2562x_get_term_curr(bq); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_VOLTAGE_NOW: val->intval = state.vbus_adc; break; case POWER_SUPPLY_PROP_CURRENT_NOW: val->intval = state.ibus_adc; break; case POWER_SUPPLY_PROP_INPUT_VOLTAGE_LIMIT: ret = bq2562x_get_input_volt_lim(bq); if (ret < 0) return ret; val->intval = ret; break; case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT: ret = bq2562x_get_input_curr_lim(bq); if (ret < 0) return ret; val->intval = ret; break; default: return -EINVAL; } return ret; } static int bq2562x_battery_get_property(struct power_supply *psy, enum power_supply_property psp, union power_supply_propval *val) { struct bq2562x_device *bq = power_supply_get_drvdata(psy); struct bq2562x_state state; int ret = 0; ret = bq2562x_get_state(bq, &state); if (ret) return ret; switch (psp) { case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT_MAX: val->intval = bq->init_data.ichg_max; break; case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE_MAX: val->intval = bq->init_data.vreg_max; break; case POWER_SUPPLY_PROP_VOLTAGE_NOW: val->intval = state.vbat_adc; break; case POWER_SUPPLY_PROP_CURRENT_NOW: val->intval = state.ibat_adc; break; default: return -EINVAL; } return ret; } static bool bq2562x_state_changed(struct bq2562x_device *bq, struct bq2562x_state *new_state) { struct bq2562x_state old_state; mutex_lock(&bq->lock); old_state = bq->state; mutex_unlock(&bq->lock); return memcmp(&old_state, new_state, sizeof(struct bq2562x_state)) != 0; } static irqreturn_t bq2562x_irq_handler_thread(int irq, void *private) { struct bq2562x_device *bq = private; struct bq2562x_state state; int ret; ret = bq2562x_get_state(bq, &state); if (ret < 0) goto irq_out; if (!bq2562x_state_changed(bq, &state)) goto irq_out; mutex_lock(&bq->lock); bq->state = state; mutex_unlock(&bq->lock); power_supply_changed(bq->charger); irq_out: return IRQ_HANDLED; } static enum power_supply_property bq2562x_power_supply_props[] = { POWER_SUPPLY_PROP_MANUFACTURER, POWER_SUPPLY_PROP_MODEL_NAME, POWER_SUPPLY_PROP_STATUS, POWER_SUPPLY_PROP_ONLINE, POWER_SUPPLY_PROP_HEALTH, POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT, POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE, POWER_SUPPLY_PROP_PRECHARGE_CURRENT, POWER_SUPPLY_PROP_CHARGE_TERM_CURRENT, POWER_SUPPLY_PROP_VOLTAGE_NOW, POWER_SUPPLY_PROP_INPUT_VOLTAGE_LIMIT, POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT, POWER_SUPPLY_PROP_CHARGE_TYPE, POWER_SUPPLY_PROP_USB_TYPE, POWER_SUPPLY_PROP_CURRENT_NOW, }; static enum power_supply_property bq2562x_battery_props[] = { POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT_MAX, POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE_MAX, POWER_SUPPLY_PROP_VOLTAGE_NOW, POWER_SUPPLY_PROP_CURRENT_NOW, }; static int bq2562x_property_is_writeable(struct power_supply *psy, enum power_supply_property prop) { switch (prop) { case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT: case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE: case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT: case POWER_SUPPLY_PROP_PRECHARGE_CURRENT: case POWER_SUPPLY_PROP_CHARGE_TERM_CURRENT: case POWER_SUPPLY_PROP_INPUT_VOLTAGE_LIMIT: return true; default: return false; } } static const struct power_supply_desc bq2562x_power_supply_desc = { .name = "bq2562x-charger", .type = POWER_SUPPLY_TYPE_USB, .usb_types = bq2562x_usb_type, .num_usb_types = ARRAY_SIZE(bq2562x_usb_type), .properties = bq2562x_power_supply_props, .num_properties = ARRAY_SIZE(bq2562x_power_supply_props), .get_property = bq2562x_get_property, .set_property = bq2562x_set_property, .property_is_writeable = bq2562x_property_is_writeable, }; static const struct power_supply_desc bq2562x_battery_desc = { .name = "bq2562x-battery", .type = POWER_SUPPLY_TYPE_BATTERY, .get_property = bq2562x_battery_get_property, .properties = bq2562x_battery_props, .num_properties = ARRAY_SIZE(bq2562x_battery_props), }; static bool bq2562x_is_volatile_reg(struct device *dev, unsigned int reg) { switch (reg) { case BQ2562X_CHRG_STAT_0...BQ2562X_FAULT_FLAG_0: case BQ2562X_ADC_IBUS_MSB...BQ2562X_ADC_TDIE_LSB: case BQ2562X_CHRG_CTRL_0: return true; default: return false; } } static const struct regmap_config bq25620_regmap_config = { .reg_bits = 8, .val_bits = 8, .max_register = BQ2562X_PART_INFO, .reg_defaults = bq25620_reg_defs, .num_reg_defaults = ARRAY_SIZE(bq25620_reg_defs), .cache_type = REGCACHE_FLAT, .volatile_reg = bq2562x_is_volatile_reg, }; static const struct regmap_config bq25622_regmap_config = { .reg_bits = 8, .val_bits = 8, .max_register = BQ2562X_PART_INFO, .reg_defaults = bq25622_reg_defs, .num_reg_defaults = ARRAY_SIZE(bq25622_reg_defs), .cache_type = REGCACHE_FLAT, .volatile_reg = bq2562x_is_volatile_reg, }; static int bq2562x_power_supply_init(struct bq2562x_device *bq, struct power_supply_config *psy_cfg, struct device *dev) { bq->charger = devm_power_supply_register(bq->dev, &bq2562x_power_supply_desc, psy_cfg); if (IS_ERR(bq->charger)) return -EINVAL; bq->battery = devm_power_supply_register(bq->dev, &bq2562x_battery_desc, psy_cfg); if (IS_ERR(bq->battery)) return -EINVAL; return 0; } static int bq2562x_hw_init(struct bq2562x_device *bq) { //struct power_supply_battery_info bat_info = { }; //TESSOLVE struct power_supply_battery_info *bat_info; int wd_reg_val = BQ2562X_WATCHDOG_DIS; int wd_max_val = BQ2562X_NUM_WD_VAL - 1; int ret = 0; int i; if (bq->watchdog_timer) { if (bq->watchdog_timer >= bq2562x_watchdog_time[wd_max_val]) wd_reg_val = wd_max_val; else { for (i = 0; i < wd_max_val; i++) { if (bq->watchdog_timer > bq2562x_watchdog_time[i] && bq->watchdog_timer < bq2562x_watchdog_time[i + 1]) { wd_reg_val = i; break; } } } } ret = regmap_update_bits(bq->regmap, BQ2562X_CHRG_CTRL_0, BQ2562X_WATCHDOG_MASK, wd_reg_val); if (ret) return ret; ret = power_supply_get_battery_info(bq->charger, &bat_info); if (ret) { dev_warn(bq->dev, "battery info missing, default values will be applied\n"); bat_info->constant_charge_current_max_ua = BQ2562X_ICHRG_I_DEF_uA; bat_info->constant_charge_voltage_max_uv = BQ2562X_VREG_V_DEF_uV; bat_info->precharge_current_ua = BQ2562X_PRECHRG_I_DEF_uA; bat_info->charge_term_current_ua = BQ2562X_TERMCHRG_I_DEF_uA; bq->init_data.ichg_max = BQ2562X_ICHRG_I_MAX_uA; bq->init_data.vreg_max = BQ2562X_VREG_V_MAX_uV; } else { bq->init_data.ichg_max = bat_info->constant_charge_current_max_ua; bq->init_data.vreg_max = bat_info->constant_charge_voltage_max_uv; } ret = bq2562x_set_ichrg_curr(bq, bat_info->constant_charge_current_max_ua); if (ret) return ret; ret = bq2562x_set_prechrg_curr(bq, bat_info->precharge_current_ua); if (ret) return ret; ret = bq2562x_set_chrg_volt(bq, bat_info->constant_charge_voltage_max_uv); if (ret) return ret; ret = bq2562x_set_term_curr(bq, bat_info->charge_term_current_ua); if (ret) return ret; ret = bq2562x_set_input_volt_lim(bq, bq->init_data.vlim); if (ret) return ret; ret = bq2562x_set_input_curr_lim(bq, bq->init_data.ilim); if (ret) return ret; power_supply_put_battery_info(bq->charger, bat_info); // TESSOLVE START ret = regmap_write(bq->regmap, BQ2562X_CHRG_CTRL_0, 0xa1); //0x16 register if (ret) return ret; ret = regmap_write(bq->regmap, BQ2562X_CHRG_CTRL_3, 0xc8); //0x19 register if (ret) return ret; //ret = regmap_write(bq->regmap, BQ2562X_NTC_CTRL_0, 0xbf); //0x1a register //if (ret) // return ret; ret = regmap_write(bq->regmap, BQ2562X_ADC_CTRL, 0xB0); //0x26 register if (ret) return ret; //TESSOLVE END return 0; } static int bq2562x_parse_dt(struct bq2562x_device *bq, struct power_supply_config *psy_cfg, struct device *dev) { int ret = 0; psy_cfg->drv_data = bq; psy_cfg->of_node = dev->of_node; ret = device_property_read_u32(bq->dev, "ti,watchdog-timeout-ms", &bq->watchdog_timer); if (ret) bq->watchdog_timer = BQ2562X_WATCHDOG_DIS; if (bq->watchdog_timer > BQ2562X_WATCHDOG_MAX || bq->watchdog_timer < BQ2562X_WATCHDOG_DIS) return -EINVAL; ret = device_property_read_u32(bq->dev, "input-voltage-limit-microvolt", &bq->init_data.vlim); if (ret) bq->init_data.vlim = BQ2562X_VINDPM_DEF_uV; if (bq->init_data.vlim > BQ2562X_VINDPM_V_MAX_uV || bq->init_data.vlim < BQ2562X_VINDPM_V_MIN_uV) return -EINVAL; ret = device_property_read_u32(bq->dev, "input-current-limit-microamp", &bq->init_data.ilim); if (ret) bq->init_data.ilim = BQ2562X_IINDPM_DEF_uA; if (bq->init_data.ilim > BQ2562X_IINDPM_I_MAX_uA || bq->init_data.ilim < BQ2562X_IINDPM_I_MIN_uA) return -EINVAL; bq->ac_detect_gpio = devm_gpiod_get_optional(bq->dev, "ac-detect", GPIOD_IN); if (IS_ERR(bq->ac_detect_gpio)) { ret = PTR_ERR(bq->ac_detect_gpio); dev_err(bq->dev, "Failed to get ac detect"); //return ret; return 0; //TESSOLVE } bq->ce_gpio = devm_gpiod_get_optional(bq->dev, "charge-enable", GPIOD_OUT_LOW); if (IS_ERR(bq->ce_gpio)) { ret = PTR_ERR(bq->ce_gpio); dev_err(bq->dev, "Failed to get ce"); //return ret; return 0; //TESSOLVE } return 0; } static int bq2562x_probe(struct i2c_client *client, const struct i2c_device_id *id) { struct device *dev = &client->dev; struct bq2562x_device *bq; struct power_supply_config psy_cfg = { }; int ret; #ifdef CONFIG_INTERRUPT_AS_GPIO int irq_gpio, irqn; #endif bq = devm_kzalloc(dev, sizeof(*bq), GFP_KERNEL); if (!bq) return -ENOMEM; bq->client = client; bq->dev = dev; mutex_init(&bq->lock); strncpy(bq->model_name, id->name, I2C_NAME_SIZE); bq->device_id = id->driver_data; switch (bq->device_id) { case BQ25620: bq->regmap = devm_regmap_init_i2c(client, &bq25620_regmap_config); break; case BQ25622: bq->regmap = devm_regmap_init_i2c(client, &bq25620_regmap_config); break; } if (IS_ERR(bq->regmap)) { dev_err(dev, "Failed to allocate register map\n"); return PTR_ERR(bq->regmap); } i2c_set_clientdata(client, bq); //TESSOLVE; start gpio_num = of_get_gpio(client->dev.of_node, 0); if (gpio_num < 0) { printk("Failed to parse GPIO number\n"); return gpio_num; } printk("GPIO number for Battery CE pin %d \n",gpio_num); // Request the GPIO pin ret = gpio_request(gpio_num, "CE-GPIO"); if (ret) { printk("Failed to request GPIO: %d\n", ret); return ret; } ret = gpio_direction_output(gpio_num, 0); if (ret) { printk("Failed to set GPIO direction/output: %d\n", ret); gpio_free(gpio_num); return ret; } //TESSOLVE END ret = bq2562x_parse_dt(bq, &psy_cfg, dev); if (ret) { dev_err(dev, "Failed to read device tree properties%d\n", ret); return ret; } ret = devm_add_action_or_reset(dev, bq2562x_charger_reset, bq); if (ret) return ret; /* OTG reporting */ bq->usb2_phy = devm_usb_get_phy(dev, USB_PHY_TYPE_USB2); if (!IS_ERR_OR_NULL(bq->usb2_phy)) { INIT_WORK(&bq->usb_work, bq2562x_usb_work); bq->usb_nb.notifier_call = bq2562x_usb_notifier; usb_register_notifier(bq->usb2_phy, &bq->usb_nb); } bq->usb3_phy = devm_usb_get_phy(dev, USB_PHY_TYPE_USB3); if (!IS_ERR_OR_NULL(bq->usb3_phy)) { INIT_WORK(&bq->usb_work, bq2562x_usb_work); bq->usb_nb.notifier_call = bq2562x_usb_notifier; usb_register_notifier(bq->usb3_phy, &bq->usb_nb); } #ifdef CONFIG_INTERRUPT_AS_GPIO irq_gpio = of_get_named_gpio(client->dev.of_node, "ti,irq-gpio", 0); if (!gpio_is_valid(irq_gpio)) { dev_err(bq->dev, "%s: %d gpio get failed\n", __func__, irq_gpio); return -EINVAL; } ret = gpio_request(irq_gpio, "bq2562x irq pin"); if (ret) { dev_err(bq->dev, "%s: %d gpio request failed\n", __func__, irq_gpio); return ret; } gpio_direction_input(irq_gpio); irqn = gpio_to_irq(irq_gpio); if (irqn < 0) { dev_err(bq->dev, "%s:%d gpio_to_irq failed\n", __func__, irqn); return irqn; } client->irq = irqn; #endif if (client->irq) { ret = devm_request_threaded_irq(dev, client->irq, NULL, bq2562x_irq_handler_thread, IRQF_TRIGGER_FALLING | IRQF_ONESHOT, dev_name(&client->dev), bq); if (ret < 0) { dev_err(dev, "get irq fail: %d\n", ret); return ret; } } ret = bq2562x_power_supply_init(bq, &psy_cfg, dev); if (ret) { dev_err(dev, "Failed to register power supply\n"); return ret; } ret = bq2562x_hw_init(bq); if (ret) { dev_err(dev, "Cannot initialize the chip.\n"); return ret; } return ret; } static const struct i2c_device_id bq2562x_i2c_ids[] = { { "bq25620", BQ25620 }, { "bq25622", BQ25622 }, {}, }; MODULE_DEVICE_TABLE(i2c, bq2562x_i2c_ids); static const struct of_device_id bq2562x_of_match[] = { { .compatible = "ti,bq25620", }, { .compatible = "ti,bq25622", }, { }, }; MODULE_DEVICE_TABLE(of, bq2562x_of_match); static const struct acpi_device_id bq2562x_acpi_match[] = { { "bq25620", BQ25620 }, { "bq25622", BQ25622 }, {}, }; MODULE_DEVICE_TABLE(acpi, bq2562x_acpi_match); static struct i2c_driver bq2562x_driver = { .driver = { .name = "bq2562x-charger", .of_match_table = bq2562x_of_match, .acpi_match_table = bq2562x_acpi_match, }, .probe = bq2562x_probe, .id_table = bq2562x_i2c_ids, }; module_i2c_driver(bq2562x_driver); MODULE_AUTHOR("Texas Instruments"); MODULE_DESCRIPTION("bq2562x charger driver"); MODULE_LICENSE("GPL v2");
DTS changes are below
bat: battery {
compatible = "simple-battery";
constant-charge-current-max-microamp = <1040000>;
constant-charge-voltage-max-microvolt = <4200000>;
precharge-current-microamp = <100000>;
charge-term-current-microamp = <60000>;
};
bq25622: charger@6b {
compatible = "ti,bq25622";
reg = <0x6b>;
pinctrl-names = "default";
pinctrl-0 = <&main_charger_pins>;
interrupt-parent = <&main_gpio0>;
gpios = <&main_gpio0 50 GPIO_ACTIVE_LOW>;
interrupts =<49 IRQ_TYPE_EDGE_FALLING>;
ti,watchdog-timeout-ms = <40000>;
input-current-limit-microamp = <1000000>;
input-voltage-limit-microvolt = <4600000>;
monitored-battery = <&bat>;
//interrupt-cells = <2>;
//ac-detect-gpios = <&main_gpio0 50 GPIO_ACTIVE_LOW>;
//charge-enable-gpios = <&main_gpio0 50 GPIO_ACTIVE_LOW>;
//ti,watchdog-timeout-ms = <40000>;
//input-current-limit-microamp = <1000000>;
//input-voltage-limit-microvolt = <4600000>;
};
Thanks,
Naresh
HI TI,
Kindly help me how to set the battery current in the driver ?
could you please help me how to set this Ibat current ?
this current (ibat_adc )shwoing zero from driver .
static int bq2562x_get_ibat_adc(struct bq2562x_device *bq)
{
int ret;
int ibat_adc_lsb, ibat_adc_msb;
u16 ibat_adc;
ret = regmap_read(bq->regmap, BQ2562X_ADC_IBAT_LSB, &ibat_adc_lsb);
if (ret)
return ret;
ret = regmap_read(bq->regmap, BQ2562X_ADC_IBAT_MSB, &ibat_adc_msb);
if (ret)
return ret;
printk("ibat_adc_lsb =%d ibat_adc_msb=%d \n", ibat_adc_lsb, ibat_adc_msb);
ibat_adc = ((ibat_adc_msb << 8) | ibat_adc_lsb) >> BQ2562X_ADC_IBAT_MOVE_STEP;
printk("ibat_adc = %d BQ2562X_ADC_IBAT_STEP_uV=%d \n" , ibat_adc, BQ2562X_ADC_IBAT_STEP_uV);
return ibat_adc * BQ2562X_ADC_IBAT_STEP_uV;
}
SUMMary :
Please help me how to set battery currentt ?
Thanks,
Naresh
Hi,
Are you able to charge when operating the board manually? Please refer to the UG at https://www.ti.com/lit/ug/sluuck2a/sluuck2a.pdf for step-by-step instructions on how to set up the charger for charging.
Thanks,
Ning.