Other Parts Discussed in Thread: BQ34Z100, MSP430FR2155
Tool/software:
Hello TI experts!
I am working on a custom designed PCB consisting of MSP430FR2155, BQ76952 and BQ34Z100. I am trying to access the data memory registers, where I am Bale to read the data from the registers but when i try to write to the registers it is not working. I took the code from the BQ799x2 example codes on TI website. I have followed the steps as mentioned in the BQ76952 TRM for accessing the data memory in the section 13.1. I will upload the codes that I am using and the screenshots of the logic analyzer as well. Could you please guide me with what could be done here?
Thanks in advance! Have a great day :)
// main program
CommandSubcommands(SET_CFGUPDATE);
BQ76952_write(monitor, EnabledProtectionsA, 0x8C, 1);
delayUS(50000);
rx_arr = BQ76952_readDMA(monitor, EnabledProtectionsA, 1);
tx_arr[6] = rx_arr[0];
tx_arr[7] = rx_arr[1];
CommandSubcommands(EXIT_CFGUPDATE);
// source code
int BQ76952_write(unsigned char Slave_address, uint16_t reg_addr, uint16_t data, int len)
{
unsigned int sentbyte = 0;
uint8_t TX_Buffer[3] = {0x00, 0x00, 0x00};
uint8_t TX_RegData[7] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
TX_RegData[0] = 0x3E;
TX_RegData[1] = reg_addr & 0xff;
TX_RegData[2] = (reg_addr >> 8) & 0xff;
TX_RegData[3] = data & 0xff; //1st byte of data
switch(len)
{
case 1: //1 byte datalength
I2CSendBytes(Slave_address, TX_RegData, 4, &sentbyte);
delayUS(2000);
TX_Buffer[0] = 0x60;
TX_Buffer[1] = Checksum(TX_RegData, 4);
TX_Buffer[2] = 0x06; //combined length of register address and data
I2CSendBytes(Slave_address, TX_Buffer, 3, &sentbyte); // Write the checksum and length
delayUS(2000);
break;
case 2: //2 byte datalength
TX_RegData[4] = (data >> 8) & 0xff;
I2CSendBytes(Slave_address, TX_RegData, 5, &sentbyte);
delayUS(2000);
TX_Buffer[0] = 0x60;
TX_Buffer[1] = Checksum(TX_RegData, 5);
TX_Buffer[2] = 0x07; //combined length of register address and data
I2CSendBytes(Slave_address, TX_Buffer, 3, &sentbyte); // Write the checksum and length
delayUS(2000);
break;
}
return 0;
}
unsigned char* BQ76952_readDMA(unsigned char Slave_address, uint16_t reg_addr, int len)
{
unsigned int sentbyte = 0;
unsigned int count = 0;
static unsigned char RX_Buffer[3] = {0x00, 0x00, 0x00};
uint8_t TX_RegData[7] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
TX_RegData[0] = 0x3E;
TX_RegData[1] = reg_addr & 0xff;
TX_RegData[2] = (reg_addr >> 8) & 0xff;
switch(len)
{
case 1: //1 byte datalength
I2CSendBytes(Slave_address, TX_RegData, 3, &sentbyte);
delayUS(2000);
I2CReadBytes(Slave_address, RX_Buffer, len, &count);
delayUS(2000);
break;
case 2: //2 byte datalength
I2CSendBytes(Slave_address, TX_RegData, 3, &sentbyte);
delayUS(2000);
I2CReadBytes(Slave_address, RX_Buffer, len, &count);
delayUS(2000);
break;
}
return RX_Buffer;
}
unsigned char Checksum(unsigned char *ptr, unsigned char len)
// Calculates the checksum when writing to a RAM register. The checksum is the inverse of the sum of the bytes.
{
unsigned char i;
unsigned char checksum = 0;
for(i=0; i<len; i++)
checksum += ptr[i];
checksum = 0xff & ~checksum;
return(checksum);
}
entering CONFIG_UPDATE mode: 
Data write : 
Checksum : 
Data read : 
exit config_update :