This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
With 2x UCD9090-Q1 in the system, the PMBus_ADDRx resistors are as follows:
Device 0:
Expected Address: 0x34
PMBus_ADDR0: 31.6kOhm
PMBus_ADDR1: 31.6kOhm
Device 1:
Expected Address: 0x41
PMBus_ADDR0: 41.2kOhm
PMBus_ADDR1: 41.2kOhm
However, when they run an I2Cscan in Linux on this I2C bus, they only get responses from addresses 0x0C and 0x7F. Even with an 8bit vs 7bit adjustment that doesn't explain these two responses. Do we know if there is any reason the UCD9090-Q1 would respond to 0x0C or 0x7F?
Thanks,
Justin
Hi, Justin,
Address 0x0C is "PMBus Alert Response" => Device responses to address 0x0C if device pull ALERT line low. Address 0x7F (127d) is prohibited, not sure why it happens. Please check your voltage on ADDR0 and ADDR1 pin, make sure they are within the voltage range as defined in ucd9090 datasheet
Regards
Anne Ngo