Tool/software:
Hello Ti,
Please check below the Schematic Attached, we are unable to get the desired outputs from the Output rails of this IC. The Schematic is designed by referring to TPS65216 PMIC Datasheet.
- We are getting the 2.5V as an output at INT_LDO pin (pin35)
- PWR_EN is supplied by 3.3V
- PFI is supplied by 0.995V
- The input supply voltage to the PMIC is 5V.