This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27427: BQ27427: Calibrating fuel gauge for given cell.

Part Number: BQ27427
Other Parts Discussed in Thread: BQSTUDIO

Tool/software: BQ Studio

We are currently using this fuel gauge in one of our new designs and we are currently facing problems in calibrating it. 

References used:

https://www.ti.com/lit/ug/sluucd5/sluucd5.pdf

https://www.tij.co.jp/jp/lit/an/slua903/slua903.pdf

Setup:

  • BQ27427 EVM  
  • Interfaced using EV2400 with BQ Studio
  • Custom Li Ion battery pack
    • Design capacity: 1250mAh
    • Discharge terminal voltage: 3000mV
    • Charging terminal voltage: 4400mV
    • Nominal voltage: 3850mV
  • Configs set using BQstudio
    • OpConfigD[Chem ID]

      3142 [10]

      Terminate voltage matches the current battery.

      Design capacity

      1250mAh

       

      Design voltage

      3850mV

       

      Charging Terminate Voltage / Taper Voltage (109)

      4400mV

       

      Taper Rate

      182 [0.1h]

      Calculation: 1250mAh = C, 62.5mA = Taper Current from datasheet.

      1250mAh / (110% x 62.5mA) = 18.18 hours. / 0.1 = 182

      Discharging Terminate Voltage

      3000mV

       

      Dsg Current Threshold

      250 [0.1h]

      Calculation: Discharge current set to 50mA. C = 1250mAh Therefore
      C / ( C / 25 x 0.1) = 250 [0.1 h]

      Chg Current Threshold

      225 [0.1h]

      Calculation: Charge current threshold set to 55.5mA. C = 1250mAh, therefore:
      C / ( C / 22.5 x 0.1) = 225[0.1 h]

      Quit Current

      313 [0.1h]

      Calculation: Set quit current even lower to 40mA. C = 1250mAh
      C / ( C / 31.25 x 0.1) = 313[0.1h]

      Dsg Relax Time

      60s

      Keeping defaults

      Chg Relax Time

      60s

      Keeping defaults

      Quit Relax Time

      1s

      Keeping defaults

      OpConfig[Temps]

      10

      Host written temperature used as temp source

      Sleep Current

      10mA

      Keeping default for the moment

Questions

  1. According to the Learning cycle reference manual, the following commands cant be found in BQstudio
    1. IT Gauge enable (0x21)
  2. The following status registers are not available
    1. GAUGE_EN
    2. RDIS
    3. QEN

That said how can I calibrate the gauge to our cell? Seems like the calibration reference guide is not valid for this Fuel gauge(BQ27427)
I want to calibrate it create a golden image so I can export the RA tables and config values.

Thank you and will be waiting for your response.

Sincerely,
Chamith