This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5149-Q1: LM5149 OCP for short circuit

Part Number: LM5149-Q1
Other Parts Discussed in Thread: LM5149,

Tool/software:

Hello, I've used the LM5149 for a design of a variable buck converter drived by a DAC. I was wondering if the hiccup mode current limiting can also protect from short circuits. From my tries the buck survives if the short has a low duration, but if i keep the wires shorted both mosfets and the LM5149 dies. My specs are:

VIN: 54V
VOUT: 50V-0.8V
IOUT: 15A

With dual-phase mode to reach 30A.

This is the schematic: