This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: new device which can work in CS topology and also has over current and short circuit protection

Part Number: LM7480-Q1
Other Parts Discussed in Thread: LM74930-Q1

Tool/software:

Hello,

in the thread LM7480-Q1: Protection against ISO7637-2 and ISO 16750-2

the user Praveen GD mentioned: "We do have a device which will be released in a couple of months which can work in CS topology and also has over current and short circuit protection. "

I'm interested in such a device too. How is the actual status? Is there a part number, datasheet etc. available?