Other Parts Discussed in Thread: UCC25630-1EVM-291, UCC28056
Tool/software:
Hi, I'm currently doing some preliminary tests on two different UCC28056BEVM-296 evaluation modules that I have.
For the test setup I'm using an AC source of 230V/50Hz and a DC Source at 12V to power the board. I'm also monitoring the output voltage using a multimeter. No load is applied to the output.
I noticed that under this condition the output voltage rises well above the nominal value of 390V reaching values of 420V and higher. I didn't check if the OVP1 trips at 440V since I'm preventively disabling the AC source when the voltage rises above 420V to avoid any possible damage to the board.
I also noticed that by applying a very small load of 0.5W the issue is resolved. The output voltage stops increasing above 390V and is somewhat stable in the 385V-391V range.
My questions are the following:
Is this the intended behavior of the controller?
If so, do I have to add a minimum load to the output of the PFC to avoid this condition?
what is the value of this minimum load?
Alternatively is the OVP1 enough to guarantee safe operation?
If this is not the intended behavior of the controller do you have any suggestions in order to solve this issue?
Moreover do you have any insight on the mechanism behind this behavior?
is it related to the stability of the system?
Thanks in advance