This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92692: Continuation of closed case

Part Number: TPS92692

Tool/software:

Regarding my closed post, I have acquired two TPS92692 evaluation board and will modify one to meet our requirements. I have a couple of questions though:
1) Why is the maximum input voltage specified as 18V? I need to run it at 20V and I cannot see a reason why not to.
2) What is the function of L1 (3.3uH ferrite)? Can it be bypassed?

Regards,

Gerry Kurz