This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65216: On powerup how to change the Default output (i.e 1.1V ) to 1.2v without using an I2C.

Part Number: TPS65216
Other Parts Discussed in Thread: USB2ANY

Tool/software:

Hello,

DCDC1 and DCDC2 generate a default output of 1.1V and  both can be adjusted via I2C (According to the Datasheet).

Can we connect an external feedback circuit to the FB2 pin of DCDC2 to produce 1.2V instead of using I2C for the adjustment?