Other Parts Discussed in Thread: BQ25756, TPS62933
Tool/software:
Hi TI,
I am designing the power converter based on BQ25758 the spec is as below
VIN=19.5V+/-5%
VOUT= USB PD EPR voltages (5V, 9V, 15V, 20V, 28V, 36V, 48V)
IOUT=5A
Switching Frequency = 450kHz.
For this I am using inductor as IHLP6767GZER5R6M11 which has below spec
Inductance = 5.6uH+/-20%
ISAT= 21A IDC_heat= 28A
DCR = 4.44mohm
I have used BQ25756 Design Calculator from TI and based on that I have chosen the inductor. However, In EVM and Datasheet the inductor chosen is 10uH, 22mohm.
I want to know can you please confirm whether the inductor which I am using is okay or not?