Other Parts Discussed in Thread: TL431, UCC28180
Tool/software:
Dear TI team,
As you know and discussed earlier also, we try to design 1000 Watt Ev Charger with ucc256601ddbr and ucc28180DR.
PFC INPUT 170 Vac to 265 Vac, 50hz
PFC OUTPUT minimum 360 Vdc ,nominal 390Vdc , maximum 410 Vdc - 3A
LLC OUTPUT DC - 64V- 15A
We are facing some problem in this design. Like it hasn't come out of burst mode. Running up to 12A in burst mode.
for reference i am attached design excel tool , schematic & waveforms with load and without load & pin levels .
Please share your voluble feedback regarding this issue.
thanks & regard
Aditya arya