Part Number: LM5100A
Other Parts Discussed in Thread: UCC21540, , UCC25600, UCC27289, UCC21520, UCC21530
Tool/software:
To whom it may concern
We want to use UCC25600, but we have a problem in design because of LM5100A which is the gate driver of this IC. We have used PSPICE version for our simulations. When we dropped LM5100A and designed LLC in open loop, the efficiency has reached near 98%. When we inserted UCC21540 as an isolated gate driver for UCC25600 and designed LLC in closed loop, the efficiency has decreased to 96%. This condition is expected. However, when we used LM5100A for isolated gate driver with UCC25600, the efficiency has reached above 100%. This condition can’t be realized in real situations. We think there is a model error related with LM5100A model in PSPICE. Do you think another error condition about this? We have added the schematic screenshot by using LM5100A. We can share the other screenshots if it is needed. We would like to know your suggestions.
Best regards,