This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part | UCC20520 | UCC21520/A | UCC21521/A/C | UCC21530 | UCC21320 | UCC20225/A | UCC21225A | UCC21220/A | UCC21222 | UCC21540/A | UCC21541 | UCC21542/A | |
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Isolation Technology | Capacitive | Capacitive | Capacitive | Capacitive | |||||||||
Viso | 5.7kVrms | 3.75kVrms | 2.5kVrms | 3.0kVrms | 5.7kVrms | ||||||||
Package | WB-16 (DW) | WB-14 (DWK) | LGA-13 | NB-16 (D) | WB-16 (DW) | WB-14 (DWK) | WB-16 (DW) | WB-14 (DWK) | |||||
Programmable Dead Time | Yes | Yes | No | Yes | Yes | No | |||||||
Input Type | PWM | INA/INB | PWM | INA/INB | INA/INB | INA/INB | |||||||
Isolation Barrier | Reinforced | Functional/Basic | Functional/Basic | Functional/Basic | Reinforced | ||||||||
Input Supply Voltage | 3V-18V | 3V-18V | 3V-5.5V | 3V-5.5V | |||||||||
Output Supply Voltage | 9.2V-25V |
9.2V-25V A: 6.5V-25V |
9.2V-25V A: 6.5V-25V C: 14.7V-25V |
14.7V-25V | 9.2V-25V |
9.2V-25V A: 6.5V-25V |
6.5V-25V |
9.2V-18V A: 6V-18V |
9.2V-18V |
9.2V-18V A: 6V-18V |
9.2V-18V |
9.2V-18V A: 6V-18V |
|
Max Working Voltage | 2121V | 792V | 990V | 1414V | |||||||||
Drive Strength(Source/Sink) | 4A/6A | 4A/6A | 4V/6A | 4A/6A | 1.5A/2.5A | 4A/6A | |||||||
Prop delay Typ | 19ns | 19ns | 28ns | 28ns | |||||||||
VDD Power-up Delay | 50us | 50us | 22us | 23us | |||||||||
UVLO | 8V | 8V/5V | 8V/5V/12V | 12V | 8V | 8V/5V | 6V | 8V/5V | 8V | 8V/5V | 8V | 8V/5V | |
Minimum CMTI | >100V/ns | >100V/ns | >100V/ns | >100V/ns | |||||||||
Channel/Channel Spacing | 2.28mm | 3.3mm | 1mm | 2.28mm | 2.28mm | 3.3mm | 2.28mm | 3.3mm | |||||
Target FETs | Si, IGBT | GaN, IGBT, Si | SiC, IGBT | Si, IGBT | GaN, Si | GaN, IGBT, Si | GaN, IGBT, Si | ||||||
Automotive grade | No | Yes | No | Yes | Yes | No | No | Yes | Yes | ||||
ENABLE/DISABLE pin | DISABLE | ENABLE | DISABLE | DISABLE | DISABLE | DISABLE |
Isolation Technology | The isolated dual channel drivers are capacitively isolated, see https://www.ti.com/isolation/capacitive-isolation.html for additional information. | ||||||||
Viso | The sinusoidal voltage that the isolator can tolerate for 60 seconds (defined in rms). | ||||||||
Package | The dual channel gate drivers come in a variety of packages which support different minimum creepage/clearance and different isolation ratings. | ||||||||
Programmable Dead time | Does the device have programmable dead time? | ||||||||
Input Type | INA/INB: Fully independent output channels. PWM: Single input to control both channels. | ||||||||
Isolation Barrier |
Reinforced means double the isolation needed to protect against electric shock and recommended for human safety. Functional/Basic means the minimum level of isolation necessary to maintain function of the device, useful for protecting other circuitry. Basic refers to isolation that has a single level of electrical protection. |
||||||||
Input Supply Voltage | The input side supply voltage range. | ||||||||
Output Supply Voltage | Output side supply voltage range. | ||||||||
Max Working Voltage | Max continuous working voltage that the isolator can withstand on a continuous basis. | ||||||||
Drive Strength(Source/Sink) | Typical peak current the device can source and sink. | ||||||||
Prop delay Typical | The reaction time between the input side and output side of the gate driver. | ||||||||
UVLO (VDD) | Output side Under voltage lockout, a watchdog for the supply voltage of the gate driver; will power down outputs when voltage is below threshold. | ||||||||
CMTI |
Max rate of change of ground potential difference that the isolator can withstand without bit errors, indicates robustness of isolator to ground noise. |
||||||||
Channel/Channel Spacing | Minimum creepage distance across package surface between Channel A and Channel B. | ||||||||
Target FETs | Typically our gate drivers are targeted for Si, SiC, IGBT, and GaN, Mosfets. We recommend using a gate driver with proper voltage range and UVLO based on the type of Mosfet being driven. | ||||||||
Automotive grade | Does this device qualify for automotive applications (AEC Q-100). | ||||||||
ENABLE/DISABLE pin | Does this device have an enable pin or disable pin? |
If you have any questions about this table, please use the "Ask a related question" button, and we will help answer them.
Best regards,
Don