Tool/software:
Dear Specialists
We are using a TPSM82816 on a custom board.
VIN, EN, and PG (p.u.) are configured to be connected to the same power supply.
Assume the following situation with the above configuration.
-VIN and EN rise instantaneously at the same time, causing PG to go high.
-The input power supply voltage is always stable.
-The conditions for PG going low shown in Table 7-2 of D/S are not met.
At this time, is it possible that PG could go low under some conditions?
(Conditions other than those shown in Table 7-2 of D/S)
Best Regards.
Ryo.