This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF35: Source impedance to the Ref35102

Part Number: REF35
Other Parts Discussed in Thread: INA118, INA826, , LM2776, LM2775,

Tool/software:

Hey,

 

we need for a new design a reference voltage with small package. The component should be used as reference voltage for the INA 826 and additional for the ADC for STM32.

In the current design we used INA118 and LM4121IM5 which is adjusted to 1,5V. For the new design we must optimize the size of the board and want used INA826 with the WSON8 packages and the reference voltage REF35102YBHR with the package BGA. In the datasheet chapter 8.3.7 reference terminal of INA826 is mentioned that: “For best performance, keep the source impedance to the REF pin less than 5 Ω“, can the reference voltage REF35102 do this? The Input bandwidth of INA is from 0Hz until 50KHz, a low noise of the complete design is very important. The INA is powered by a dual voltage of +5V and -3.2V.

The Ref35 is powered by +3.3V.
The voltage of +5.5V is generated by the IC LM2775 and the voltage -3,2V by LM2776, both components and Ref35102 is powered by LM3603

Or can you support us another component with a small package.

TI site recommended the REF35 as alternate to LM4121IM5-1.2.

The reference design REF35EVM was ordered

Thank you for your support