Tool/software:
Hello,
I read that i can swap the polarity of the SS TX RX lines, so i swapped the polarity on pins 17 16 and pins 21 20 (See picture)
Is it also possible to then swap polarity at the output pins? pins 6 and 7 and pins 9 and 10
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
I read that i can swap the polarity of the SS TX RX lines, so i swapped the polarity on pins 17 16 and pins 21 20 (See picture)
Is it also possible to then swap polarity at the output pins? pins 6 and 7 and pins 9 and 10
Hi Erwin:
polarity swap is allowed for USB3 spec, so you can swap pin 6/7 and 9/10 as well.
Best
Brian