Other Parts Discussed in Thread: BQSTUDIO, EV2400
Tool/software:
Hi,
I am no longer able to UNSEAL my batteries.
When I follow the procedure, SEC1 and SEC0 behave normally until I click on NEW_BATTERY.
I click on UNSEAL:
I click on UNSEAL_FULL_ACCESS:
I click on NEW_BATTERY:
Then I receive the following message: WriteMACReadBlock communication error: First two bytes of MAC response read from the device do not match the MAC command sent.
I read on the forum that the command still went through and that I should continue, which I did.
To activate the EOS mode, I then write:
I receive the following message: Operation failed because initial read of all data flash failed.
PS: I have the latest versions of the EV2400 and BQStudio
Is there a command to be done to resolve the problem?
Best regards
MARQUET Lilian