Tool/software:
Hi all!
I've been struggling with getting BQ24610 to work in my product. One of few problems I encountered is this:
I use BQ24610 to charge 6xLiIon battery pack. I use power adapter fine-adjusted to exactly 26.5V, and after back-power preventing schottky diode, BQ charger 'sees' 26.2VDC.
With resistor dividers I set V_BAT=24.44V, I_CHARGE=1.05A, I_TERM=0.28A.
Right now I'm looking at my PCB, and I measure battery pack current = 83mA, and battery pack voltage = 24.93V. So if I correctly understand datasheet p. "9.3.5 Charge Termination, Recharge, and Safety Timer":
When VTTC is valid, termination is detected while the voltage on the VFB pin is higher than the VRECH threshold AND the charge current is less than the ITERM threshold.
VRECH for my divider is 23.85V (50mV drop on VFB). So what is going on? Both conditions are met. Charging should be terminated, but is not. When I leave it for few more hours, a TTC timer will kick in and indeed terminate the charge, and signal it properly (STAT1 = STAT2 = off). I have TTC timer set for 4:40h. Is there something I'm missing?
One might say: maybe your VFB resistor divider is not accurate enough (1% resistors), and you are not really above VRECHG threshold. Ok, if so, then why did BQ decided to end the fastcharge current regulation and drop the current from full charge 1.05A down to tens of mA?
Anyone has idea why this might happen? Or is it just me not understanding datasheet?
Cheers,
Mateusz