Other Parts Discussed in Thread: TPS22991, TPS22995, BQ2970
Tool/software:
For a battery charger based on the BQ2562X, where a battery "pack" is inserted into the charger by the user, and the user must press a button to begin charging: when the button is pressed, I am considering using a load switch to connect the battery to the BQ2562X. Candidates are TPS22991, TPS22995, TPS22996.
My question is if these load switches will be transparent enough to the BQ2562X to allow it to operate as intended, or if having the battery connected to the BQ2562X via load switch would interfere with the operation of the BQ2562X.