Other Parts Discussed in Thread: LM5171, LM5170
Tool/software:
Hello
I am studying the operation of the LM5170-Q board in Boost mode. I have closed the pins according to the manual and have shorted the 2 pad breakers on the back of the board. I supplied a voltage of 12 V to the LV side, while the HV side of the board is connected with Power resistor 30 ohm, 3000W. However, I encountered an issue where the output voltage on the HV side is only 11.719 V and the Boost mode LED in the top right corner is not illuminated., whereas I expected it to be around 48-50 V as specified in the manual.
The pins I have shorted: J2, J3, J4, J5, J8, J21, J25, J28, J29, J34, J35, J36, and J37.