This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi All,
We used the LM3644 to drive LED in Torch mode.
But we find the torch mode can't be set at some devices.
We have checked the schematic, the Torch pin and Strobe pin are floating.
Do those two pins need to be connect to "High"?
Or have any idea for this problem?
Thank you.
Zeno
Hi John,
Thank you for your reply.
The Enable registor value :
Set Enable Register => 0b10001011 (0x88) ,
but read the Enable registor value is :
Read Enable Register => 0b10000011 (0x83)
And we read the Fault flag (0x0A &0B), the flag value :
Read Flag1: 0x80 (0x0A)
Read Flag2: 0x02 (0x0B)
Thank you.
Zeno
Hi Zeno,
In torch mode you used, you could leave Torch pin and Strobe pin floating. It should work.
It is very weird that the OVP fault bit is 1 in 0x0B register. There might be LED open happening when turn on the current, or the LED VF is too large. Could please show me the LED you are using? Could you please capture a waveform at that moment?
Thanks!
Best,
John.