Tool/software:
This is a follow-up for the thread at
I now have a BQ25120AEVM and have further information about this issue which still needs resolving. I am able to reproduce the issue with the EVM (by soldering capacitors between the output power plane and GND plane) so this should allow support to replicate and analyze the issue better.
Large capacitive loads cause the issue and the amount of capacitive load needed to produce the issue greatly varies between BQ chips installed.
The following images show the waveform of the BQ25120AEVM under different conditions:
1. BQ25120AEVM with 8.2K load resistor:
This is the expected switching behavior since the is no capacitive load.
2. BQ25120AEVM with "good" BQ chip with 8.2K load resistor and 3 to 5 22uF caps load:
The caps have little effect on BQ switching behavior and only reduce ripple as expected. "good" BQ units function normally with even 5 or 6 x 22uF caps.
3. BQ25120AEVM with "bad" BQ chip installed and with 8.2K load resistor and 3 to 5 22uF caps load:
Different BQ chips show this switching behavior with different capacitive loads. Some have normal switching behavior with even 6 22uF caps while some show the switching behavior below with only 3x 22uF caps.
We want to avoid this BQ switching behavior since it causes much larger ripple. On our custom PCB design we use 3x 22uF caps in addition to various smaller decoupling caps and about 15% of BQ chips exhibit the noisy switching behavior above.