Other Parts Discussed in Thread: TPS560430
Tool/software:
Dear Support,
We want to simulate FRA (AC Bode plot) operation of LMR54410(F), but operating in constant current mode, with current-sense amplifier in feedback loop. Something similar to the schematic below:
(Please note that this schematic uses a similar TPS560430 and the model is only for transient simulation, not AC. The load is modeled as an LED with a dynamic resistance of 2.432 Ohms.)
Do you have an AC model available for the LMR54410(F)? Or any similar IC? We are currently using TINA, but what format the model will be in is a secondary consideration.
Our configuration with current-sense amplifier and low dynamic load resistance, drastically changes the feedback loop compared to the controller in standard CV mode. We want to perform AC analysis to select the proper components to compensate for loop stability. The transicnt analysis unfortunately takes a very long time and in no way fully answers how specific compensation components affect stability.
Thank you in advance for any help.