This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25148: Initially design this device for up to a 12A load. But having issues starting up the regulator with a light load. I need a reliable start up with a low power load of 30-40 mA.

Part Number: LM25148


Tool/software:

Initially design this device for up to a 12A load.  But having issues starting up the regulator with a light load.

I need a reliable start up with a low power load of 30-40 mA.  Is that possible?  I can start up with 130mA and once started I can lower the load down to 10 mA or even no load.

Any ideas.