This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM8S6C24: PMBus

Part Number: TPSM8S6C24

Tool/software:

Hi All,

I have a question about the TPSM8S6C24.
Is it possible to read the output voltage and current using PMBus??


Best Regards,
Ishiwata

  •  

    Is it possible to read the output voltage and current using PMBus??

    Yes.  The commands are READ_VOUT (Command code 8Bh) and READ_IOUT (Command Code 8Ch)

    READ_VOUT uses Linear16 encoding, as defined by VOUT_MODE (Command Code 20h)

    READ_IOUT uses Linear11 encoding, as defined by the PMBus specification.

    Both commands use the READ_WORD SMBus transaction type.