This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear team,
Customer want to know if they can enable ship mode with adapter present? I checked the D/S seems ship mode only active with battery only. Is there a way to turn off ship FET with adapter?
If yes, please let the customer know to set the regs.
They have tested:
without adapter,REG14 SFET_PRESENT - 1h, REG11 SDRV_CTRL_1:0 - 2h,-> SDRV_DLY -0 or 1, can enter shipmode。
with adapter,配置SFET_PRESENT为1h,SDRV_CTRL_1:0为2h,SDRV_DLY -0 or 1h -> remove adapter, cannot enter shipmode;
Thank you.
Charles